<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>HoverGames Drone ChallengeのトピックMAVLink Console Command Help</title>
    <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/MAVLink-Console-Command-Help/m-p/1402072#M158</link>
    <description>&lt;P&gt;I am working on trying to send commands via the MAVLink Console on the QGroundControl Software to manually control the Hovergames PX4 Quadcopter. I saw a link of various commands for MAVLink, but I am not sure how to write the specified commands in the console. For example, I would like my drone to roll left or right at a rate of 4.5 radians per second, as well as pitching forward front or back at a rate of 4.5 radians per second. This would occur after takeoff at a resting height of around 1.5 meters. An example of the list of commands is attached to an image below. I understand what each variable means, but my coding skills with MAVLink are at a beginner level.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 19 Jan 2022 21:10:51 GMT</pubDate>
    <dc:creator>loganlamm17</dc:creator>
    <dc:date>2022-01-19T21:10:51Z</dc:date>
    <item>
      <title>MAVLink Console Command Help</title>
      <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/MAVLink-Console-Command-Help/m-p/1402072#M158</link>
      <description>&lt;P&gt;I am working on trying to send commands via the MAVLink Console on the QGroundControl Software to manually control the Hovergames PX4 Quadcopter. I saw a link of various commands for MAVLink, but I am not sure how to write the specified commands in the console. For example, I would like my drone to roll left or right at a rate of 4.5 radians per second, as well as pitching forward front or back at a rate of 4.5 radians per second. This would occur after takeoff at a resting height of around 1.5 meters. An example of the list of commands is attached to an image below. I understand what each variable means, but my coding skills with MAVLink are at a beginner level.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jan 2022 21:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/HoverGames-Drone-Challenge/MAVLink-Console-Command-Help/m-p/1402072#M158</guid>
      <dc:creator>loganlamm17</dc:creator>
      <dc:date>2022-01-19T21:10:51Z</dc:date>
    </item>
  </channel>
</rss>