<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: QGC PX4 Firmware Issue in HoverGames Drone Challenge</title>
    <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/QGC-PX4-Firmware-Issue/m-p/1401210#M157</link>
    <description>&lt;P&gt;I was able to retry installing the bootloader via the JLink debugger. I made sure to write 0x0 after including the file name for the loadbin command. This fixed the issue of connecting the FMU to the QGC Software.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 19 Jan 2022 01:15:19 GMT</pubDate>
    <dc:creator>loganlamm17</dc:creator>
    <dc:date>2022-01-19T01:15:19Z</dc:date>
    <item>
      <title>QGC PX4 Firmware Issue</title>
      <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/QGC-PX4-Firmware-Issue/m-p/1399331#M155</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I recently finished uploading the bootloader and JLink debugging code into the FMU. I followed the process that was provided by the NXP Hovergames drone tutorial, and downloaded the QGC software to connect to the drone; thus input individual code with MAVLink. However, I ran into an issue with trying to upgrade the firmware and connect to the software. The message came up where the FMU time-ed out trying to connect to the software. I believe one issue is that I haven't used an updated QGC application since I downloaded it in October of 2021. I used the same bin codes from the NXP site, so I don't believe there is an issue with the binary codes for the firmware. What is the possible solution to this? I am so close to completing my project, and I don't want to be held back because of this.&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 07:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/HoverGames-Drone-Challenge/QGC-PX4-Firmware-Issue/m-p/1399331#M155</guid>
      <dc:creator>loganlamm17</dc:creator>
      <dc:date>2022-01-14T07:15:52Z</dc:date>
    </item>
    <item>
      <title>Re: QGC PX4 Firmware Issue</title>
      <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/QGC-PX4-Firmware-Issue/m-p/1400778#M156</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Does the&amp;nbsp;&lt;A href="https://nxp.gitbook.io/hovergames/userguide/troubleshooting" target="_self"&gt;Troubleshooting&lt;/A&gt; fix this issue? I will move this question to&amp;nbsp;&lt;SPAN class="lia-link-navigation lia-link-disabled"&gt;&lt;A href="https://community.nxp.com/t5/HoverGames-Drone-Challenge/bd-p/hovergames-drone-challenge/page/2" target="_self"&gt;HoverGames Drone Challenge&lt;/A&gt; community.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jan 2022 08:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/HoverGames-Drone-Challenge/QGC-PX4-Firmware-Issue/m-p/1400778#M156</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2022-01-18T08:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: QGC PX4 Firmware Issue</title>
      <link>https://community.nxp.com/t5/HoverGames-Drone-Challenge/QGC-PX4-Firmware-Issue/m-p/1401210#M157</link>
      <description>&lt;P&gt;I was able to retry installing the bootloader via the JLink debugger. I made sure to write 0x0 after including the file name for the loadbin command. This fixed the issue of connecting the FMU to the QGC Software.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jan 2022 01:15:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/HoverGames-Drone-Challenge/QGC-PX4-Firmware-Issue/m-p/1401210#M157</guid>
      <dc:creator>loganlamm17</dc:creator>
      <dc:date>2022-01-19T01:15:19Z</dc:date>
    </item>
  </channel>
</rss>