<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Confusing datasheet NAFE33352 in High Performance Analog Front End Interfaces</title>
    <link>https://community.nxp.com/t5/High-Performance-Analog-Front/Confusing-datasheet-NAFE33352/m-p/2418795#M218</link>
    <description>&lt;P&gt;Good day,&lt;BR /&gt;my task is to characterize and test the NAFE33352 for potential later use, but have difficulty following or locating some information in the following datasheet. &lt;A href="https://www.nxp.com/docs/en/data-sheet/NAFE33352.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/NAFE33352.pdf&lt;/A&gt;&lt;BR /&gt;Until now, after just glancing over the most important functionalities, I have the following problems/questions in no specific order:&lt;/P&gt;&lt;P&gt;a) 7.6.3 HV Input:&lt;BR /&gt;For single-ended analog measurements the datasheet says to configure the LVMUX like this:&lt;BR /&gt;HV input positive: AI1P, Isense&lt;BR /&gt;HV input positive: AI1N, Vsense&lt;/P&gt;&lt;P&gt;I can't find those configurations in Table 12. With a bit of fantasy, the first could be 00010/b, assuming Vsense is VSNS. But the second combination doesn't seem to exist. Even if they existed, do I just have to tie the three SENSE pins down to GND?&lt;BR /&gt;How else can I measure AI1P and AI1N vs GND? I need two single-ended channels for my application.&lt;/P&gt;&lt;P&gt;b) 7.6.6 Analog inputs to low-voltage multiplexer (LV_MUX)&lt;BR /&gt;Table 12, what is VCM? The COM input of the MUX seen in Figure 1? Is the COM the common mode output level for the differential PGAs? Can I use COM as reference for my single-ended measurements?&lt;/P&gt;&lt;P&gt;c) 5 Block diagram&lt;BR /&gt;Why are there 2 LS inputs per MUX and what do the mean? How can the outputs of the AMPs of DAC and VSENSE be connected together?&lt;/P&gt;&lt;P&gt;d) 7.5.8 Voltage sources polarity switching (AC excitation)&lt;BR /&gt;What happened to VIEX_CHOP? It's only mentioned twice in this section but never where to find it and in which register to set it.&lt;/P&gt;&lt;P&gt;e) 7.14 CMD_MM, multichannel multireading command&lt;BR /&gt;How do I configure the respective registers, which channels can I choose from? Does this chip not only have a 2-channel ADC? Where can I find the CH_CONFIGx registers that are mentioned in the section?&lt;BR /&gt;Also Table 20 mentions DATA0...DATA7 for up to 8 channels but no more information what this means? Are the combinations of Table 12 considered channels?&lt;/P&gt;&lt;P&gt;It may be that some information I'm looking for is somewhere in the datasheet, but even if that is the case, it is well hidden or a different terminology/abbreviation is used, which makes it even more confusing and hard to find.&lt;BR /&gt;If I want to use this IC, I would need to order an eval-board as soon as possible, but I can't with so many open questions and not knowing if it's even possible to do what I try to do with the chip. In a nutshell, one analog input and 2 independent analog input channels.&lt;BR /&gt;Hoping to hear from you soon. Best regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Tue, 06 Oct 2026 14:48:07 GMT</pubDate>
    <dc:creator>InterestedUser</dc:creator>
    <dc:date>2026-10-06T14:48:07Z</dc:date>
    <item>
      <title>Confusing datasheet NAFE33352</title>
      <link>https://community.nxp.com/t5/High-Performance-Analog-Front/Confusing-datasheet-NAFE33352/m-p/2418795#M218</link>
      <description>&lt;P&gt;Good day,&lt;BR /&gt;my task is to characterize and test the NAFE33352 for potential later use, but have difficulty following or locating some information in the following datasheet. &lt;A href="https://www.nxp.com/docs/en/data-sheet/NAFE33352.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/NAFE33352.pdf&lt;/A&gt;&lt;BR /&gt;Until now, after just glancing over the most important functionalities, I have the following problems/questions in no specific order:&lt;/P&gt;&lt;P&gt;a) 7.6.3 HV Input:&lt;BR /&gt;For single-ended analog measurements the datasheet says to configure the LVMUX like this:&lt;BR /&gt;HV input positive: AI1P, Isense&lt;BR /&gt;HV input positive: AI1N, Vsense&lt;/P&gt;&lt;P&gt;I can't find those configurations in Table 12. With a bit of fantasy, the first could be 00010/b, assuming Vsense is VSNS. But the second combination doesn't seem to exist. Even if they existed, do I just have to tie the three SENSE pins down to GND?&lt;BR /&gt;How else can I measure AI1P and AI1N vs GND? I need two single-ended channels for my application.&lt;/P&gt;&lt;P&gt;b) 7.6.6 Analog inputs to low-voltage multiplexer (LV_MUX)&lt;BR /&gt;Table 12, what is VCM? The COM input of the MUX seen in Figure 1? Is the COM the common mode output level for the differential PGAs? Can I use COM as reference for my single-ended measurements?&lt;/P&gt;&lt;P&gt;c) 5 Block diagram&lt;BR /&gt;Why are there 2 LS inputs per MUX and what do the mean? How can the outputs of the AMPs of DAC and VSENSE be connected together?&lt;/P&gt;&lt;P&gt;d) 7.5.8 Voltage sources polarity switching (AC excitation)&lt;BR /&gt;What happened to VIEX_CHOP? It's only mentioned twice in this section but never where to find it and in which register to set it.&lt;/P&gt;&lt;P&gt;e) 7.14 CMD_MM, multichannel multireading command&lt;BR /&gt;How do I configure the respective registers, which channels can I choose from? Does this chip not only have a 2-channel ADC? Where can I find the CH_CONFIGx registers that are mentioned in the section?&lt;BR /&gt;Also Table 20 mentions DATA0...DATA7 for up to 8 channels but no more information what this means? Are the combinations of Table 12 considered channels?&lt;/P&gt;&lt;P&gt;It may be that some information I'm looking for is somewhere in the datasheet, but even if that is the case, it is well hidden or a different terminology/abbreviation is used, which makes it even more confusing and hard to find.&lt;BR /&gt;If I want to use this IC, I would need to order an eval-board as soon as possible, but I can't with so many open questions and not knowing if it's even possible to do what I try to do with the chip. In a nutshell, one analog input and 2 independent analog input channels.&lt;BR /&gt;Hoping to hear from you soon. Best regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Tue, 06 Oct 2026 14:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/High-Performance-Analog-Front/Confusing-datasheet-NAFE33352/m-p/2418795#M218</guid>
      <dc:creator>InterestedUser</dc:creator>
      <dc:date>2026-10-06T14:48:07Z</dc:date>
    </item>
    <item>
      <title>Re: Confusing datasheet NAFE33352</title>
      <link>https://community.nxp.com/t5/High-Performance-Analog-Front/Confusing-datasheet-NAFE33352/m-p/2419184#M219</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;a)&amp;nbsp;AI1P and AI1N can be used as two independent single-ended inputs (IN_SEL = 00100 and 00101). Connect the external signal return to AGND. They share the same ADC, so measurements are sequential.&amp;nbsp;The valid configurations are:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="ErikaC_0-1791404436327.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/397456i430918750193AF21/image-size/medium?v=v2&amp;amp;px=400" role="button" title="ErikaC_0-1791404436327.png" alt="ErikaC_0-1791404436327.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;b)VCM and COM are internal signals, not external reference pins. For single-ended measurements, connect the signal return to AGND.&lt;/P&gt;
&lt;P&gt;c)The two LS blocks are internal level shifters for the positive and negative MUX paths. They do not represent additional external inputs.&lt;/P&gt;
&lt;P&gt;d) The polarity-chopping function is configured through AIO_CHOP[7:6] in AI_CONFIG2 (0x22). Set AIO_CHOP = 11b for DAC polarity chopping with two averaged ADC readings.&lt;/P&gt;
&lt;P&gt;e)&amp;nbsp;The device supports 8 logical channels (CH0–CH7) sharing the same ADC. Each logical channel can have its own input and ADC configuration, is enabled through AI_MULTI_CH_EN, and has a corresponding AI_DATA0–AI_DATA7 result register.&lt;/P&gt;
&lt;P&gt;Hope this helps!&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2026 20:27:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/High-Performance-Analog-Front/Confusing-datasheet-NAFE33352/m-p/2419184#M219</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2026-10-07T20:27:48Z</dc:date>
    </item>
  </channel>
</rss>