<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>High Performance Analog Front End InterfacesのトピックPCA9306: Supplying same 3.3V voltage to VREF1 and VREF2</title>
    <link>https://community.nxp.com/t5/High-Performance-Analog-Front/PCA9306-Supplying-same-3-3V-voltage-to-VREF1-and-VREF2/m-p/2177094#M144</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Is it possible to use PCA9306 with both sides at 3.3V to disconnect I2C buses? Or is there a better solution? Speed is not critical, there will be just 4 slaves on the device side of the bus, other side connected to a pair of GPIOs.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 29 Sep 2025 01:27:19 GMT</pubDate>
    <dc:creator>yterada</dc:creator>
    <dc:date>2025-09-29T01:27:19Z</dc:date>
    <item>
      <title>PCA9306: Supplying same 3.3V voltage to VREF1 and VREF2</title>
      <link>https://community.nxp.com/t5/High-Performance-Analog-Front/PCA9306-Supplying-same-3-3V-voltage-to-VREF1-and-VREF2/m-p/2177094#M144</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Is it possible to use PCA9306 with both sides at 3.3V to disconnect I2C buses? Or is there a better solution? Speed is not critical, there will be just 4 slaves on the device side of the bus, other side connected to a pair of GPIOs.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 01:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/High-Performance-Analog-Front/PCA9306-Supplying-same-3-3V-voltage-to-VREF1-and-VREF2/m-p/2177094#M144</guid>
      <dc:creator>yterada</dc:creator>
      <dc:date>2025-09-29T01:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9306: Supplying same 3.3V voltage to VREF1 and VREF2</title>
      <link>https://community.nxp.com/t5/High-Performance-Analog-Front/PCA9306-Supplying-same-3-3V-voltage-to-VREF1-and-VREF2/m-p/2177171#M145</link>
      <description>&lt;P&gt;You can evaluate the PCA9617A.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Sep 2025 05:28:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/High-Performance-Analog-Front/PCA9306-Supplying-same-3-3V-voltage-to-VREF1-and-VREF2/m-p/2177171#M145</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-09-29T05:28:57Z</dc:date>
    </item>
  </channel>
</rss>