<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>High Performance Analog Front End InterfacesのトピックRe: Short circuit protection for PCA9615?</title>
    <link>https://community.nxp.com/t5/High-Performance-Analog-Front/Short-circuit-protection-for-PCA9615/m-p/2148467#M134</link>
    <description>&lt;P&gt;No,it doesn't have the short circuit protection,I don't recommend you do that!&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Aug 2025 12:11:58 GMT</pubDate>
    <dc:creator>guoweisun</dc:creator>
    <dc:date>2025-08-07T12:11:58Z</dc:date>
    <item>
      <title>Short circuit protection for PCA9615?</title>
      <link>https://community.nxp.com/t5/High-Performance-Analog-Front/Short-circuit-protection-for-PCA9615/m-p/2147889#M133</link>
      <description>&lt;P&gt;I am considering using the #PCA9615 in an environment where the DSDAM, DSDAP, DSCLP, and DSCLM pins could be shorted, either to each other, to VDDB, or to GND, in a controlled, recoverable, fault condition. Given the fact that this chip is designed to drive low impedance loads, I am wondering if these pins include short circuit protection?&amp;nbsp; Would use of the EN input for Hot Swap when anticipating the fault help the chip to survive this situation? Thanks for your help&lt;/P&gt;&lt;P&gt;Best regards, Patrick&lt;/P&gt;</description>
      <pubDate>Thu, 07 Aug 2025 00:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/High-Performance-Analog-Front/Short-circuit-protection-for-PCA9615/m-p/2147889#M133</guid>
      <dc:creator>JPM6</dc:creator>
      <dc:date>2025-08-07T00:04:17Z</dc:date>
    </item>
    <item>
      <title>Re: Short circuit protection for PCA9615?</title>
      <link>https://community.nxp.com/t5/High-Performance-Analog-Front/Short-circuit-protection-for-PCA9615/m-p/2148467#M134</link>
      <description>&lt;P&gt;No,it doesn't have the short circuit protection,I don't recommend you do that!&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Aug 2025 12:11:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/High-Performance-Analog-Front/Short-circuit-protection-for-PCA9615/m-p/2148467#M134</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2025-08-07T12:11:58Z</dc:date>
    </item>
  </channel>
</rss>