<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: I can't install freemaster 3.0</title>
    <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009300#M91</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having the same issue.&amp;nbsp; I've tried all of the suggested workarounds.&amp;nbsp; I've checked that java is up to date.&amp;nbsp; I've checked that windows is up to date.&amp;nbsp; I have FreeMASTER 2.5 installed but I'm having issues using it with the S32K144EVB.&amp;nbsp; It sees the board and seems to connect but then I don't see anything happening.&amp;nbsp; I may be misusing the software though.&amp;nbsp; I will start a new thread on that if needed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Running:&lt;/P&gt;&lt;P&gt;Windows 10 1809 (64bit)&lt;/P&gt;&lt;P&gt;Java Version 1.8 Update 241 (b07)&lt;/P&gt;&lt;P&gt;Intel Xeon E3-1505M v6&lt;/P&gt;&lt;P&gt;64Gig Ram&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would attach my log file but none is created unless I try running the installation again and the get error of already having an installation instance running.&amp;nbsp; That log file shows up and details that error.&amp;nbsp; Yes I've extracted both folders.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would also mention that I've downloaded it twice in case of file corruption.&amp;nbsp; I've also had our IT guy log in and try to install.&amp;nbsp; He tried installing on his machine and had the same issue.&amp;nbsp; I've had 3 other people in my department try installing it and all have the EXACT same outcome as me.&amp;nbsp; No log files created until trying to run a second instance of installer.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you for your time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Feb 2020 16:45:30 GMT</pubDate>
    <dc:creator>sparkee</dc:creator>
    <dc:date>2020-02-21T16:45:30Z</dc:date>
    <item>
      <title>I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009279#M70</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm having some difficulties installing freemaster 3.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A installanywhere window appears after I double click&amp;nbsp;FMASTERSW30.exe. After its completion bar finishes, a window with the freemaster logo appears for about one second. Then, nothing else happens.&lt;/P&gt;&lt;P&gt;I'm using windows 7 and java is updated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I try to run the installer again, a multiple launches error appears and a log file is generated at&amp;nbsp;C:\NXP\FreeMASTER 3.0\_FreeMASTER_installation\Logs. But no log is generated for the first try.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone facing this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2020 15:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009279#M70</guid>
      <dc:creator>geansousa</dc:creator>
      <dc:date>2020-02-10T15:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009280#M71</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gean,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please confirm weather you have administrative privileges on the PC you are trying to install FreeMASTER on. The installer contains a built-in JRE&amp;nbsp;and does not require nor affect&amp;nbsp;any existing Java distributions on the system.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's quite strange that it creates a folder on your C driver which happens only after user confirms installation options. Meaning it requires user input on the following screen:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture3.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103661i20FC37C81B489267/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture3.PNG" alt="Capture3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Prior to this one all processing happens in a temporary directory.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it your first time installing FreeMASTER 3.0 on that PC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you redownload the installer (in case it got corrupted) and try running it again.&amp;nbsp;If it get's blocked make sure&amp;nbsp;to terminate any previously&amp;nbsp;launched processes before a new attempt:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103360i79F5E9611E884354/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In case it still persists could you provide additional information on your OS and PC specifications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Feb 2020 17:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009280#M71</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-10T17:20:54Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009281#M72</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have exactly the same problem. After a brief display of the FreeMASTER logo, nothing else happens. I can see this running proccess of &lt;SPAN&gt;Free&lt;/SPAN&gt;&lt;SPAN&gt;MASTER:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="p.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97825iBE6C847DA8EF5B03/image-size/large?v=v2&amp;amp;px=999" role="button" title="p.png" alt="p.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Advice please&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Tomas&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 06:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009281#M72</guid>
      <dc:creator>tomas_bubela</dc:creator>
      <dc:date>2020-02-13T06:41:29Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009282#M73</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are sorry for the inconveniences. We are currently investigating this issue and will post updates on this thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 09:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009282#M73</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-13T09:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009283#M74</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/geansousa"&gt;geansousa&lt;/A&gt;,&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/tomas.bubela@centrum.cz"&gt;tomas.bubela@centrum.cz&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please try the following:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Unzip the installer on your hard drive. You should be able to see the following two folders - &lt;STRONG&gt;InstallerData&lt;/STRONG&gt; and &lt;STRONG&gt;Windows&lt;/STRONG&gt;.&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture1.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97757iF6AB3F405B9DA8BB/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture1.PNG" alt="Capture1.PNG" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;LI&gt;Navigate to &lt;STRONG&gt;Windows&amp;nbsp;&lt;/STRONG&gt;folder, it's content should look like this:&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture2.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97865iEF680508814A3DB2/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture2.PNG" alt="Capture2.PNG" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;LI&gt;Open a console terminal and execute the following command (make sure there are no other installer processes running in the background):&lt;BR /&gt;&lt;STRONG&gt;&amp;gt; "FreeMASTER 3.0.exe" LAX_VM resource\jre\bin\java.exe&lt;/STRONG&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let us know if this helps. In case of failure do you get any errors in the console ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Iulian&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 10:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009283#M74</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-13T10:14:58Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009284#M75</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is ok now.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 11:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009284#M75</guid>
      <dc:creator>tomas_bubela</dc:creator>
      <dc:date>2020-02-13T11:45:00Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009285#M76</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm facing the same problem and also the solution posted by Iulian&amp;nbsp;does not solve my problem.&lt;/P&gt;&lt;P&gt;I'm runnig on Win7 pc with java version 1.8.0241, the system is fully update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 13:52:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009285#M76</guid>
      <dc:creator>d_dicerto</dc:creator>
      <dc:date>2020-02-14T13:52:03Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009286#M77</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/d.dicerto@gmail.com"&gt;d.dicerto@gmail.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately we are still unable to reproduce this issue on our side so I&amp;nbsp;would like to clarify some minor details:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;When running the command in the terminal are you facing the exact same behavior ?&lt;/LI&gt;&lt;LI&gt;If you run it repeatedly do you get "Another installation in progress" error ?&lt;/LI&gt;&lt;LI&gt;Are you extracting both folders from &lt;STRONG&gt;FMATERSW30.exe&lt;/STRONG&gt; ?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please try running it with your version of java, just replace the the path to &lt;STRONG&gt;java.exe&lt;/STRONG&gt;, ex:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; &lt;STRONG&gt;"FreeMASTER 3.0.exe" LAX_VM "C:\Program Files\Java\jre1.8.0_241\bin\java.exe".&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 15:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009286#M77</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-14T15:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009287#M78</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Iulian&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Yes, in the terminal i'm facing the exact same behavior&lt;/LI&gt;&lt;LI&gt;Yes, I've got the "Another installation" error&lt;/LI&gt;&lt;LI&gt;Yes, I extracted both folders&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Ok, running the command you suggest works like a charm.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot and have a nice day&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 16:03:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009287#M78</guid>
      <dc:creator>d_dicerto</dc:creator>
      <dc:date>2020-02-14T16:03:44Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009288#M79</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am also having problem installing. Installations asked for an activation code. I provided the code received from the NXP support portal, and received an error message &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Error Initializing activation Library. Licensing Service not installed. (FNP error 20)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 19:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009288#M79</guid>
      <dc:creator>sushil_prabhu</dc:creator>
      <dc:date>2020-02-14T19:51:31Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009289#M80</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/sushil.prabhu@sparton.com"&gt;sushil.prabhu@sparton.com&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that this one is caused by &lt;STRONG&gt;FlexNet Licensing Service&lt;/STRONG&gt; - either&amp;nbsp;due to&amp;nbsp;installation failure or OS restriction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could check if it was installed on your system:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is there a &lt;STRONG&gt;FlexNet&lt;/STRONG&gt; entry in your system services list ?&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture3.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100625i6D78D045E7253FD0/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture3.PNG" alt="Capture3.PNG" /&gt;&lt;/span&gt;&lt;/LI&gt;&lt;LI&gt;Was the service executable installed in &lt;STRONG&gt;Program Files&lt;/STRONG&gt; ? &lt;BR /&gt;It's path should be:&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;C:\Program Files (x86)\Common Files\Macrovision Shared\FlexNet Publisher&lt;/STRONG&gt;&lt;/EM&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If one of those holds could you start the service manually and reattempt the installation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you also provide your installation log (&lt;EM style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;C&lt;/STRONG&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;&lt;EM style="border: 0px; font-weight: inherit;"&gt;:\&lt;/EM&gt;NXP\FreeMASTER 3.0\_FreeMASTER_installation\Logs&lt;/STRONG&gt;&lt;/EM&gt;).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 09:15:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009289#M80</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-17T09:15:21Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009290#M81</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Julian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for this information. FlexNet Licensing Service was not running on my PC. I started it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, it is 64 bit and the service executable is installed in&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Program Files\Common Files\Macrovision Shared\FlexNet Publisher&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Installation of the FreeMaster failed with the same error message. How can I get this working?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sushil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 15:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009290#M81</guid>
      <dc:creator>sushil_prabhu</dc:creator>
      <dc:date>2020-02-17T15:04:12Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009291#M82</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Unfortunately it should've been a 32 bit version service. I'm looking into this one and will keep you posted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 15:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009291#M82</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-17T15:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009292#M83</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/sushil.prabhu@sparton.com"&gt;sushil.prabhu@sparton.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was unable to reproduce this issue. Could you please provide installation log file for further investigation ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 08:41:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009292#M83</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-18T08:41:33Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009293#M84</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;P&gt;Where can find the installation log file?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sushil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 14:14:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009293#M84</guid>
      <dc:creator>sushil_prabhu</dc:creator>
      <dc:date>2020-02-18T14:14:56Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009294#M85</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Logs default location&amp;nbsp;-&amp;nbsp;&lt;EM style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;C&lt;/STRONG&gt;&lt;STRONG style="border: 0px; font-weight: bold;"&gt;&lt;EM style="border: 0px; font-weight: inherit;"&gt;:\&lt;/EM&gt;NXP\FreeMASTER 3.0\_FreeMASTER_installation\Logs.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;DIV style="position: absolute; left: 187px; top: 6.54545px;"&gt;&lt;DIV class="gtx-trans-icon"&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 14:35:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009294#M85</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-18T14:35:00Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009295#M86</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have tried installing few times. Please see the attached logs.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 14:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009295#M86</guid>
      <dc:creator>sushil_prabhu</dc:creator>
      <dc:date>2020-02-18T14:41:20Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009296#M87</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/sushil.prabhu@sparton.com"&gt;sushil.prabhu@sparton.com&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In both cases your installation fails due to limited privileges. Here's the error message from your logs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;CLLReason [errorNo=5, errorString=Error installing the FlexNet Publisher Licensing Service and registers.&lt;STRONG&gt; Access has been denied to a resource, either a service or a file, or the registry. Administrator privilege is required to resolve this problem&lt;/STRONG&gt;. (FNP error 1007), flxActMajorErrorNo=0, flxActMinorErrorNo=0, flxActSysErrorNo=0, flxCommErrorNo=1007]&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unless you run the installer as admin&amp;nbsp;you won't be able to use FreeMASTER Lite.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that only the Lite feature requires license validation. You can try installing&amp;nbsp;FreeMASTER (main tool) by deselecting FreeMASTER Lite option on the Component Selection screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 15:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009296#M87</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-02-18T15:38:25Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009297#M88</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, our company has IT managing the installation. So when they tried to install from my account and used their admin credentials when prompted, it did not work. When IT logged in as admin and installed the application, installation went through without any issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sushil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2020 17:19:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009297#M88</guid>
      <dc:creator>sushil_prabhu</dc:creator>
      <dc:date>2020-02-18T17:19:45Z</dc:date>
    </item>
    <item>
      <title>Re: I can't install freemaster 3.0</title>
      <link>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009298#M89</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;P&gt;Do you have an example code that runs on IMXRT1064 that can be connected from the FreeMaster? It is not clear to me what is needed on the target in order for Free Master to communicate.  I am going through the user guides, but some pointers may help me figure out things quicker. I am using MCUxpresso 11.1.0 and SDK 2.6.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sushil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2020 15:33:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/I-can-t-install-freemaster-3-0/m-p/1009298#M89</guid>
      <dc:creator>sushil_prabhu</dc:creator>
      <dc:date>2020-02-20T15:33:36Z</dc:date>
    </item>
  </channel>
</rss>