<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: FreeMASTER Segger RTT communication plugin</title>
    <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1419232#M891</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34487"&gt;@MichalH&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;The telnet connectivity test is successful on my side as well, with the same output you get. At this point it is probably something on target side. The RS-232 comm works fine though.&lt;/P&gt;&lt;P&gt;Anyway I think I am loosing interest for this SEGGER RTT connectivity option. Do I read correctly &lt;A href="https://www.segger.com/products/debug-probes/j-link/technology/about-real-time-transfer/" target="_self"&gt;here&lt;/A&gt; that it achieves 1 Mbps? That's not very fast actually. I was looking for a way to speed up large recorder downloads. Maybe I should focus on TCP/UDP instead. Would you agree?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;</description>
    <pubDate>Thu, 24 Feb 2022 16:23:17 GMT</pubDate>
    <dc:creator>lucabarbiero</dc:creator>
    <dc:date>2022-02-24T16:23:17Z</dc:date>
    <item>
      <title>FreeMASTER Segger RTT communication plugin</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1416893#M889</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to use the new Segger RTT communication plugin. Of course I am running the latest freemaster target driver with net transport and segger_rtt. This is my freemaster_cfg.h:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lucabarbiero_0-1645460809741.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171243iF787433CBB08B268/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lucabarbiero_0-1645460809741.png" alt="lucabarbiero_0-1645460809741.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From the host I want to establish a connection in passive mode. Therefore I have an active J-Link debug session with the command line debugger:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lucabarbiero_0-1645460419982.png" style="width: 465px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171238iCB927885B2871CFD/image-dimensions/465x460?v=v2" width="465" height="460" role="button" title="lucabarbiero_0-1645460419982.png" alt="lucabarbiero_0-1645460419982.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But freemaster app says target unreachable:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lucabarbiero_1-1645460491243.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/171240iC03708F00A68075C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lucabarbiero_1-1645460491243.png" alt="lucabarbiero_1-1645460491243.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;What should I look into? Can it be a problem to establish a telnet connection to localhost:19021? Because I think telnet is not enabled in my computer (and I need to reach out to my IT to get it enabled). Or is there a telnet client embedded in freemaster?&lt;/P&gt;&lt;P&gt;Or do you think the problem is something else?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;</description>
      <pubDate>Mon, 21 Feb 2022 16:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1416893#M889</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2022-02-21T16:27:01Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER Segger RTT communication plugin</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1417480#M890</link>
      <description>&lt;P&gt;Dear Luca,&lt;/P&gt;
&lt;P&gt;your steps and JLink.exe screenshot look correct. As soon as the JLink.exe connects to the device, it also starts the RTT server at port 19021 and is ready to accept connections.&lt;/P&gt;
&lt;P&gt;FreeMASTER does not depend on having telnet installed in system.&amp;nbsp;It uses an internal TCP connection directly. However,&amp;nbsp;the telnet utility is quite useful to test if the RTT server is reachable. There are also other tools like TeraTerm which are able to connect by telnet/TCP link.&lt;/P&gt;
&lt;P&gt;In my case, I'm able to connect with telnet and I get the following "welcome" message:&lt;/P&gt;
&lt;PRE&gt;&lt;STRONG&gt;&amp;gt; telnet localhost 19021&lt;/STRONG&gt;&lt;BR /&gt;SEGGER J-Link V7.56d - Real time terminal output &lt;BR /&gt;J-Link OpenSDA compiled May 27 2019 10:59:53 V1.0, SN=621000000 &lt;BR /&gt;Process: JLink.exe &lt;/PRE&gt;
&lt;P&gt;It would be good if you could verify the connectivity the same way. I think the local firewall or antivirus software may block the incoming connection even for localhost clients (like FreeMASTER).&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Tue, 22 Feb 2022 12:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1417480#M890</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-02-22T12:27:29Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER Segger RTT communication plugin</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1419232#M891</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34487"&gt;@MichalH&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;The telnet connectivity test is successful on my side as well, with the same output you get. At this point it is probably something on target side. The RS-232 comm works fine though.&lt;/P&gt;&lt;P&gt;Anyway I think I am loosing interest for this SEGGER RTT connectivity option. Do I read correctly &lt;A href="https://www.segger.com/products/debug-probes/j-link/technology/about-real-time-transfer/" target="_self"&gt;here&lt;/A&gt; that it achieves 1 Mbps? That's not very fast actually. I was looking for a way to speed up large recorder downloads. Maybe I should focus on TCP/UDP instead. Would you agree?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 16:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1419232#M891</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2022-02-24T16:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER Segger RTT communication plugin</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1419592#M892</link>
      <description>&lt;P&gt;Dear Luca,&lt;/P&gt;
&lt;P&gt;I'm sorry for the issues with the RTT. Can you give it one more try with &lt;A href="https://drive.google.com/file/d/1ts9r-V9Or0QXzZAQLzZ2ylXe5cvi5K6j/view?usp=sharing" target="_blank" rel="noopener"&gt;this patch&lt;/A&gt;&amp;nbsp;of mcbpgi.dll copied over the existing file in&amp;nbsp;"c:\NXP\FreeMASTER 3.1\FreeMASTER\mcbpgi.dll" ?&amp;nbsp; The failure Test Connection message will now also print an error code number. This number will tell if there is a problem with a localhost "telnet" connection or with the target interface.&lt;/P&gt;
&lt;P&gt;Also, make sure you have the target side configured as&amp;nbsp;&lt;/P&gt;
&lt;PRE&gt;#define FMSTR_TRANSPORT FMSTR_NET // Use network transport layer&lt;BR /&gt;#define FMSTR_NET_DRV FMSTR_NET_SEGGER_RTT // Use network driver for SEGGER RTT&amp;nbsp;&lt;/PRE&gt;
&lt;P&gt;..and you have the RTT C files in project (src\support\segger_rtt\*.c) . There are fmstr_rtt examples available in MCUXPresso SDK packages for FRDM-K64F and i.MX-RT10xx.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Anyway,&amp;nbsp;the fastest options are definitely the USB-CDC and TCP/UDP options.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your cooperation,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 25 Feb 2022 07:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1419592#M892</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-02-25T07:09:59Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER Segger RTT communication plugin</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1423768#M906</link>
      <description>&lt;P&gt;Hi Michal, sorry for the delay. I can confirm all the settings on target side you mentioned. Now with the same setup as described before, but with your modified DLL, I get the error code displayed in the screenshot. What does it tell you?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lucabarbiero_0-1646640820996.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/172600i119487585EAD002D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lucabarbiero_0-1646640820996.png" alt="lucabarbiero_0-1646640820996.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;From here I don't have interest in making this work, I don't think I will use it. It's not particularly fast as you confirm, and this communication channel&amp;nbsp; only works in poll mode, which not compatible with my application. In my use case I found that long interrupt is the way to go.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 08:18:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1423768#M906</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2022-03-07T08:18:36Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER Segger RTT communication plugin</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1423777#M907</link>
      <description>&lt;P&gt;Dear Luca,&lt;/P&gt;
&lt;P&gt;thanks for making the experiment. The error code says there was a timeout when waiting for the response. This means the TCP/telnet connection to JLink.exe was established well. The timeout occurs during the communication over RTT itself. It would need some more debugging of the MCU side to find out what is wrong.&lt;/P&gt;
&lt;P&gt;It is okay if you do not want to spend more time with it. Still this forum thread may be helpful for someone trying to make the same connection.&lt;/P&gt;
&lt;P&gt;Please close this thread.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 08:34:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1423777#M907</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-03-07T08:34:35Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER Segger RTT communication plugin</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1423778#M908</link>
      <description>&lt;P&gt;Ok so there must be something in my embedded software application. For this experiment I was calling FMSTR_Poll() as the only task in my infinite loop. But I also have another fast interrupt where my control loop executes. Maybe that is interfering.&amp;nbsp; I am accepting your solution as there seems to be no issue with FreeMASTER desktop app, using SEGGER RTT communication channel in passive mode. Thanks for your support!&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 08:40:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-Segger-RTT-communication-plugin/m-p/1423778#M908</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2022-03-07T08:40:34Z</dc:date>
    </item>
  </channel>
</rss>