<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed. in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Upgrade-issue-IFATAL-ERROR-Removing-earlier-version-while/m-p/1403154#M864</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just tried an upgrade from previous 3.1 version to the latest, but I'm not successful.&lt;/P&gt;&lt;P&gt;The installation itself is started, then it tries to remove previous version, but that is the point when it fails.&lt;/P&gt;&lt;P&gt;The original folder is empty (seems to be removed), I also cannot see it in the system list of installed apps, but the new installer sees it somehow (probably in registers).&lt;/P&gt;&lt;P&gt;Is there any way to make a clean installation, overriding the registry check? Or which registers should I "remove" before the installation starts?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
    <pubDate>Fri, 21 Jan 2022 09:12:33 GMT</pubDate>
    <dc:creator>matejpacha_Ineltech</dc:creator>
    <dc:date>2022-01-21T09:12:33Z</dc:date>
    <item>
      <title>Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Upgrade-issue-IFATAL-ERROR-Removing-earlier-version-while/m-p/1403154#M864</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just tried an upgrade from previous 3.1 version to the latest, but I'm not successful.&lt;/P&gt;&lt;P&gt;The installation itself is started, then it tries to remove previous version, but that is the point when it fails.&lt;/P&gt;&lt;P&gt;The original folder is empty (seems to be removed), I also cannot see it in the system list of installed apps, but the new installer sees it somehow (probably in registers).&lt;/P&gt;&lt;P&gt;Is there any way to make a clean installation, overriding the registry check? Or which registers should I "remove" before the installation starts?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 09:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Upgrade-issue-IFATAL-ERROR-Removing-earlier-version-while/m-p/1403154#M864</guid>
      <dc:creator>matejpacha_Ineltech</dc:creator>
      <dc:date>2022-01-21T09:12:33Z</dc:date>
    </item>
    <item>
      <title>Re: Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Upgrade-issue-IFATAL-ERROR-Removing-earlier-version-while/m-p/1403193#M866</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/191647"&gt;@matejpacha_Ineltech&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you check this &lt;A href="https://community.nxp.com/t5/FreeMASTER/My-Win10-can-not-install-FreeMaster3-1-2/m-p/1315039/highlight/true#M669" target="_self"&gt;thread.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Hope it helps,&lt;BR /&gt;Iulian&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 10:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Upgrade-issue-IFATAL-ERROR-Removing-earlier-version-while/m-p/1403193#M866</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2022-01-21T10:13:46Z</dc:date>
    </item>
    <item>
      <title>Re: Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Upgrade-issue-IFATAL-ERROR-Removing-earlier-version-while/m-p/1403316#M869</link>
      <description>&lt;P&gt;Sorry for duplicated thread, I did search for it and did found nothing like that.&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 15:33:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Upgrade-issue-IFATAL-ERROR-Removing-earlier-version-while/m-p/1403316#M869</guid>
      <dc:creator>matejpacha_Ineltech</dc:creator>
      <dc:date>2022-01-21T15:33:28Z</dc:date>
    </item>
  </channel>
</rss>