<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic COM handshake forced by FreeMASTER? in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1362305#M784</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I came arround an issue with FTDI used on a custom board, featuring RTS and CTS signals to control a bootloader process. I have tested a common terminal program (Hercules from hw.cz), which opens the COM port with no HW control and communicates with the MCU correctly. However, when I try to open COM port communication using FreeMASTER, the RTS signal is forced on and the MCU goes to reset (thus no communication is detected by FreeMASTER app). Temporarily I can remove the signals from the FTDI on the PCB, however, I would appreciate if the handshake signals can be configured in the FreeMASTER settings (if I disable handshake signals in the driver settings, FreeMASTER forces them back to enable and the issue persists). I understand that handshake signals are recommended for Windows users as it keeps the communication with FTDI-based devices alive. However, in this particular case it prevents the communication enitrely.&lt;/P&gt;&lt;P&gt;If there is any workaround, please let me know.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
    <pubDate>Wed, 27 Oct 2021 09:00:55 GMT</pubDate>
    <dc:creator>matejpacha_Ineltech</dc:creator>
    <dc:date>2021-10-27T09:00:55Z</dc:date>
    <item>
      <title>COM handshake forced by FreeMASTER?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1362305#M784</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I came arround an issue with FTDI used on a custom board, featuring RTS and CTS signals to control a bootloader process. I have tested a common terminal program (Hercules from hw.cz), which opens the COM port with no HW control and communicates with the MCU correctly. However, when I try to open COM port communication using FreeMASTER, the RTS signal is forced on and the MCU goes to reset (thus no communication is detected by FreeMASTER app). Temporarily I can remove the signals from the FTDI on the PCB, however, I would appreciate if the handshake signals can be configured in the FreeMASTER settings (if I disable handshake signals in the driver settings, FreeMASTER forces them back to enable and the issue persists). I understand that handshake signals are recommended for Windows users as it keeps the communication with FTDI-based devices alive. However, in this particular case it prevents the communication enitrely.&lt;/P&gt;&lt;P&gt;If there is any workaround, please let me know.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 09:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1362305#M784</guid>
      <dc:creator>matejpacha_Ineltech</dc:creator>
      <dc:date>2021-10-27T09:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: COM handshake forced by FreeMASTER?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1362493#M788</link>
      <description>&lt;P&gt;Ahoj Mateji,&lt;/P&gt;
&lt;P&gt;I confirm the RTS control is enabled by FreeMASTER which means the Windows will automatically assert the signal when opening the port.&lt;/P&gt;
&lt;P&gt;We will make the feature configurable in next version. Actually, as the 3.1.3 is already at the door, so this change will make it to 3.1.4 early next year. There might be a prototype version earlier, I would inform you in this thread.&lt;/P&gt;
&lt;P&gt;Thanks for this 'new feature' proposal.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 14:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1362493#M788</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2021-10-27T14:22:30Z</dc:date>
    </item>
    <item>
      <title>Re: COM handshake forced by FreeMASTER?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1363003#M789</link>
      <description>&lt;P&gt;Ahoj Michale,&lt;/P&gt;&lt;P&gt;thank you for considering it in the future release. It's highly appreciated!&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
      <pubDate>Thu, 28 Oct 2021 06:42:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1363003#M789</guid>
      <dc:creator>matejpacha_Ineltech</dc:creator>
      <dc:date>2021-10-28T06:42:07Z</dc:date>
    </item>
    <item>
      <title>Re: COM handshake forced by FreeMASTER?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1403306#M868</link>
      <description>&lt;P&gt;Ahoj Michale,&lt;/P&gt;&lt;P&gt;just curious if there is any early prototype available?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 15:18:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1403306#M868</guid>
      <dc:creator>matejpacha_Ineltech</dc:creator>
      <dc:date>2022-01-21T15:18:23Z</dc:date>
    </item>
    <item>
      <title>Re: COM handshake forced by FreeMASTER?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1403381#M870</link>
      <description>&lt;P&gt;Ahoj Mateji,&lt;/P&gt;
&lt;P&gt;yes, this feature is already implemented in 3.1.4 prototype and will be released during March 2022. Please contact me directly at &lt;A href="mailto:michal.hanak@nxp.com" target="_blank"&gt;michal.hanak@nxp.com&lt;/A&gt;&amp;nbsp;to discuss how we can test the feature together.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Fri, 21 Jan 2022 17:59:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/COM-handshake-forced-by-FreeMASTER/m-p/1403381#M870</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-01-21T17:59:13Z</dc:date>
    </item>
  </channel>
</rss>