<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Blinky with FreeMASTER? in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Blinky-with-FreeMASTER/m-p/1228186#M626</link>
    <description>&lt;P&gt;Never mind, I figured it out.&amp;nbsp; I missed the part where he linked FreeMASTER to Blinky by pointing it to the ELF/DWARF file.&lt;/P&gt;</description>
    <pubDate>Mon, 08 Feb 2021 18:22:28 GMT</pubDate>
    <dc:creator>GaryOlmstead</dc:creator>
    <dc:date>2021-02-08T18:22:28Z</dc:date>
    <item>
      <title>Blinky with FreeMASTER?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Blinky-with-FreeMASTER/m-p/1228173#M625</link>
      <description>&lt;P&gt;I have MCUXpresso 11.3.0 and SDK 2.9 for the KV31F.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm watching part one of the FreeMASTER webinar, and the narrator has a demo program that is Blinky but also with FreeMASTER code.&amp;nbsp; I don't see that on my version.&amp;nbsp; The only FreeMASTER examples are a simple BDM demo and the same thing with a UART.&amp;nbsp; For the KV31F SDK, the Blinky demo does not have FreeMASTER built in, and the Import Wizard skips over the page that allows adding middle ware.&lt;/P&gt;&lt;P&gt;So how do you create this project?&amp;nbsp; Or did I mess up the SDK?&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 17:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Blinky-with-FreeMASTER/m-p/1228173#M625</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2021-02-08T17:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: Blinky with FreeMASTER?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Blinky-with-FreeMASTER/m-p/1228186#M626</link>
      <description>&lt;P&gt;Never mind, I figured it out.&amp;nbsp; I missed the part where he linked FreeMASTER to Blinky by pointing it to the ELF/DWARF file.&lt;/P&gt;</description>
      <pubDate>Mon, 08 Feb 2021 18:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Blinky-with-FreeMASTER/m-p/1228186#M626</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2021-02-08T18:22:28Z</dc:date>
    </item>
  </channel>
</rss>