<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Location of PCANBasic.dll in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Location-of-PCANBasic-dll/m-p/1262263#M613</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;make sure you are using the 32-bit version of the &lt;STRONG&gt;PCANBasic.dll&lt;/STRONG&gt; with FreeMASTER. It should be enough to put it to&amp;nbsp;&lt;STRONG&gt;c:\Windows\SysWOW64&lt;/STRONG&gt; folder. To be sure, you can also store the DLL in "c:\NXP\FreeMASTER 3.1\FreeMASTER\plugins\can" next to the &lt;STRONG&gt;focpgi.dll&lt;/STRONG&gt;&amp;nbsp;file which is the main FreeMASTER-over-CAN plug-in executable.&lt;/P&gt;
&lt;P&gt;You can use the Microsoft &lt;A href="https://docs.microsoft.com/en-us/sysinternals/downloads/sigcheck" target="_self"&gt;sigcheck&lt;/A&gt; tool to find out if your file is 32 or 64 bit version. In my case, it says:&lt;/P&gt;
&lt;PRE&gt;sigcheck.exe C:\Windows\SysWOW64\PCANBasic.dll&lt;BR /&gt;&lt;BR /&gt;Sigcheck v2.80 - File version and signature viewer&lt;BR /&gt;Copyright (C) 2004-2020 Mark Russinovich&lt;BR /&gt;Sysinternals - www.sysinternals.com&lt;BR /&gt;&lt;BR /&gt;c:\windows\syswow64\PCANBasic.dll:&lt;BR /&gt;Verified: Signed&lt;BR /&gt;Signing date: 15:58 11/20/2019&lt;BR /&gt;Publisher: PEAK-System Technik GmbH&lt;BR /&gt;Company: PEAK-System Technik GmbH&lt;BR /&gt;Description: PCAN-Basic API Library, 32-bit&lt;BR /&gt;Product: PCAN-Basic API&lt;BR /&gt;Prod version: 4.4&lt;BR /&gt;File version: 4.4.0.288&lt;BR /&gt;MachineType: &lt;STRONG&gt;32-bit&lt;/STRONG&gt;&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Apr 2021 18:44:48 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2021-04-14T18:44:48Z</dc:date>
    <item>
      <title>Location of PCANBasic.dll</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Location-of-PCANBasic-dll/m-p/1262111#M612</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to connect to a S32K144EVB via the CANbus, using a PEAK CAN-to-USB connector. When I try to configure the connection in FreeMASTER, the PEAK option says the driver isn't found.&lt;/P&gt;&lt;P&gt;I've put the .dll in both Windows/System32 and Windows/SysWOW64, per the instructions in the readme from PEAK, and FreeMASTER still reports it can't find it. The installation of the api for PEAK didn't create a PEAK directory, at the top level nor in either Program Files directory.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm running the example CAN model&amp;nbsp;flexcan_and_fm_over_can_s32k14x.slx from the NXP MBDT examples, and using the FreeMASTER project provided,&amp;nbsp;flexcan_and_fm_over_can_s32k14x.pmp.&lt;/P&gt;&lt;P&gt;How can I get the FreeMASTER project to find the PEAK .dll? Where do I put the .dll?&lt;/P&gt;&lt;P&gt;Thanks much.&lt;/P&gt;&lt;P&gt;--Nancy&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 15:31:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Location-of-PCANBasic-dll/m-p/1262111#M612</guid>
      <dc:creator>neffnan</dc:creator>
      <dc:date>2021-04-14T15:31:37Z</dc:date>
    </item>
    <item>
      <title>Re: Location of PCANBasic.dll</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Location-of-PCANBasic-dll/m-p/1262263#M613</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;make sure you are using the 32-bit version of the &lt;STRONG&gt;PCANBasic.dll&lt;/STRONG&gt; with FreeMASTER. It should be enough to put it to&amp;nbsp;&lt;STRONG&gt;c:\Windows\SysWOW64&lt;/STRONG&gt; folder. To be sure, you can also store the DLL in "c:\NXP\FreeMASTER 3.1\FreeMASTER\plugins\can" next to the &lt;STRONG&gt;focpgi.dll&lt;/STRONG&gt;&amp;nbsp;file which is the main FreeMASTER-over-CAN plug-in executable.&lt;/P&gt;
&lt;P&gt;You can use the Microsoft &lt;A href="https://docs.microsoft.com/en-us/sysinternals/downloads/sigcheck" target="_self"&gt;sigcheck&lt;/A&gt; tool to find out if your file is 32 or 64 bit version. In my case, it says:&lt;/P&gt;
&lt;PRE&gt;sigcheck.exe C:\Windows\SysWOW64\PCANBasic.dll&lt;BR /&gt;&lt;BR /&gt;Sigcheck v2.80 - File version and signature viewer&lt;BR /&gt;Copyright (C) 2004-2020 Mark Russinovich&lt;BR /&gt;Sysinternals - www.sysinternals.com&lt;BR /&gt;&lt;BR /&gt;c:\windows\syswow64\PCANBasic.dll:&lt;BR /&gt;Verified: Signed&lt;BR /&gt;Signing date: 15:58 11/20/2019&lt;BR /&gt;Publisher: PEAK-System Technik GmbH&lt;BR /&gt;Company: PEAK-System Technik GmbH&lt;BR /&gt;Description: PCAN-Basic API Library, 32-bit&lt;BR /&gt;Product: PCAN-Basic API&lt;BR /&gt;Prod version: 4.4&lt;BR /&gt;File version: 4.4.0.288&lt;BR /&gt;MachineType: &lt;STRONG&gt;32-bit&lt;/STRONG&gt;&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 18:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Location-of-PCANBasic-dll/m-p/1262263#M613</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2021-04-14T18:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: Location of PCANBasic.dll</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Location-of-PCANBasic-dll/m-p/1263729#M620</link>
      <description>&lt;P&gt;Thanks, Michal. That indeed fixed it.&amp;nbsp; --Nancy&lt;/P&gt;</description>
      <pubDate>Fri, 16 Apr 2021 19:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Location-of-PCANBasic-dll/m-p/1263729#M620</guid>
      <dc:creator>neffnan</dc:creator>
      <dc:date>2021-04-16T19:28:52Z</dc:date>
    </item>
  </channel>
</rss>