<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USBDM won't work with Freemaster or KDS in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/USBDM-won-t-work-with-Freemaster-or-KDS/m-p/1004243#M60</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Lance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, FreeMASTER 3.0 has removed support for USBDM&amp;nbsp;interface&amp;nbsp;due to licensing issues. Installing FreeMASTER 3.0 also disables the USBDM access in FreeMASTER 2.x versions. The only way to&amp;nbsp;keep using USBDM with FreeMASTER is to uninstall 3.0 and re-install 2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest FreeMASTER 3.0.1 (and the upcoming 3.0.2) contains the latest P&amp;amp;E Micro, Segger j-Link and ARM CMSIS-DAP interface libraries. Use of debugging probes&amp;nbsp;from one of these vendors should be quite straightforward replacement for USBDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry I have no better answer,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Mar 2020 15:48:41 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2020-03-09T15:48:41Z</dc:date>
    <item>
      <title>USBDM won't work with Freemaster or KDS</title>
      <link>https://community.nxp.com/t5/FreeMASTER/USBDM-won-t-work-with-Freemaster-or-KDS/m-p/1004242#M59</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On one of my Windows 10 computers I cannot get USBDM to work with Freemaster (version 2.0 or 3.0) or KDS (3.2.&amp;nbsp; I've tried reinstalling Freemaster and the USBDM drivers and utilities with no effect.&amp;nbsp; The USBDM utilities (ARM GDB server, ARM Programmer) work fine so it appears there's nothing wrong with the drivers or adapter.&amp;nbsp; When I attempt to connect using plug-in "FreeMASTER BDM Communication Plug-in "CoretxM, PowerPC, HSC08/12,&amp;nbsp;Coldfire" the USBDM option is greyed out in the Config dialog box.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also cannot get the KDS debugger to connect via the USBDM adapter.&amp;nbsp; I am able to configure and launch a Debug session and the specific USBDM adapter serial# appears in the "BDM Selection" pull-down but the launch terminates with:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Error with command: gdb --version&lt;BR /&gt;Cannot run program "gdb": Launching failed"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The same hardware and software are working on a couple other computers in my lab all of which are running the same Win 10 OS.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2020 15:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/USBDM-won-t-work-with-Freemaster-or-KDS/m-p/1004242#M59</guid>
      <dc:creator>lancefisher</dc:creator>
      <dc:date>2020-03-09T15:35:23Z</dc:date>
    </item>
    <item>
      <title>Re: USBDM won't work with Freemaster or KDS</title>
      <link>https://community.nxp.com/t5/FreeMASTER/USBDM-won-t-work-with-Freemaster-or-KDS/m-p/1004243#M60</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Lance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, FreeMASTER 3.0 has removed support for USBDM&amp;nbsp;interface&amp;nbsp;due to licensing issues. Installing FreeMASTER 3.0 also disables the USBDM access in FreeMASTER 2.x versions. The only way to&amp;nbsp;keep using USBDM with FreeMASTER is to uninstall 3.0 and re-install 2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The latest FreeMASTER 3.0.1 (and the upcoming 3.0.2) contains the latest P&amp;amp;E Micro, Segger j-Link and ARM CMSIS-DAP interface libraries. Use of debugging probes&amp;nbsp;from one of these vendors should be quite straightforward replacement for USBDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm sorry I have no better answer,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2020 15:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/USBDM-won-t-work-with-Freemaster-or-KDS/m-p/1004243#M60</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-03-09T15:48:41Z</dc:date>
    </item>
  </channel>
</rss>