<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Connect s32k148 with Freemaster in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Connect-s32k148-with-Freemaster/m-p/998786#M58</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fermin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what I see you need to sort out the connectivity issue first (which at this point is not FreeMASTER related).&lt;/P&gt;&lt;P&gt;First things I would suggest to check:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="http://www.pemicro.com/opensda/"&gt;PEDrivers&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/quick-reference-guide/S32K148EVB-QSG.pdf"&gt;Board setup&lt;/A&gt; (page 8)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;It is indeed as&amp;nbsp;you guessed - when the target is properly connected you should be able to see on OpenSDA entry in the COM ports list. Another drivers check - you should be able to see an additionally mounted memory device in "My Computer" (it's usually called EVB-S32K148).&lt;/P&gt;&lt;P&gt;Once you sort it out you can try connecting to the board, for this you can check the following &lt;A _jive_internal="true" href="https://community.nxp.com/videos/8895"&gt;video&amp;nbsp;&lt;/A&gt;(starting at min 1:15).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Mar 2020 13:49:41 GMT</pubDate>
    <dc:creator>iulian_stan</dc:creator>
    <dc:date>2020-03-06T13:49:41Z</dc:date>
    <item>
      <title>Connect s32k148 with Freemaster</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Connect-s32k148-with-Freemaster/m-p/998785#M57</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I'm currently trying to connect the platform s32k148 with Freemaster with no luck. I have installed FreeMASTER Communication Driver and Freemaster 3.0. However, when I try to connect to the platform using the connection wizard in FreeMASTER I'm not sure how to configure the connection. Moreover, in the Device Administrator I can see that there is some issue with the drivers. If I understand correctly, the platform should be linked to some COM port, so when I download the code after build I use the same COM port (I have been using the OpenSDA interface for downloading the code to the platform).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96361i673A3372B0FE31C4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any help or links to guide me in the process is much appreciated. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Fermin Chico&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 12:53:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Connect-s32k148-with-Freemaster/m-p/998785#M57</guid>
      <dc:creator>fmendozad</dc:creator>
      <dc:date>2020-03-06T12:53:49Z</dc:date>
    </item>
    <item>
      <title>Re: Connect s32k148 with Freemaster</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Connect-s32k148-with-Freemaster/m-p/998786#M58</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Fermin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what I see you need to sort out the connectivity issue first (which at this point is not FreeMASTER related).&lt;/P&gt;&lt;P&gt;First things I would suggest to check:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="http://www.pemicro.com/opensda/"&gt;PEDrivers&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/quick-reference-guide/S32K148EVB-QSG.pdf"&gt;Board setup&lt;/A&gt; (page 8)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;It is indeed as&amp;nbsp;you guessed - when the target is properly connected you should be able to see on OpenSDA entry in the COM ports list. Another drivers check - you should be able to see an additionally mounted memory device in "My Computer" (it's usually called EVB-S32K148).&lt;/P&gt;&lt;P&gt;Once you sort it out you can try connecting to the board, for this you can check the following &lt;A _jive_internal="true" href="https://community.nxp.com/videos/8895"&gt;video&amp;nbsp;&lt;/A&gt;(starting at min 1:15).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2020 13:49:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Connect-s32k148-with-Freemaster/m-p/998786#M58</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-03-06T13:49:41Z</dc:date>
    </item>
  </channel>
</rss>