<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 Where is MCAT?</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Where-is-MCAT/m-p/1229518#M571</link>
    <description>&lt;P&gt;I give up.&amp;nbsp; Where are you hiding MCAT?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have MCUXpresso 11.3, KV31F SDK v2.9, and FreeMASTER 3.1.&amp;nbsp; It isn't in any of them. It's supposed to be a plug-in for FreeMASTER, but it isn't on any menu, and the help files have never heard of it.&lt;/P&gt;&lt;P&gt;I have AN4642,AN4870 and AN4912, which all assume MCAT is already running.&lt;/P&gt;&lt;P&gt;So, where is it?&lt;/P&gt;</description>
    <pubDate>Wed, 10 Feb 2021 19:29:21 GMT</pubDate>
    <dc:creator>GaryOlmstead</dc:creator>
    <dc:date>2021-02-10T19:29:21Z</dc:date>
    <item>
      <title>Where is MCAT?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Where-is-MCAT/m-p/1229518#M571</link>
      <description>&lt;P&gt;I give up.&amp;nbsp; Where are you hiding MCAT?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have MCUXpresso 11.3, KV31F SDK v2.9, and FreeMASTER 3.1.&amp;nbsp; It isn't in any of them. It's supposed to be a plug-in for FreeMASTER, but it isn't on any menu, and the help files have never heard of it.&lt;/P&gt;&lt;P&gt;I have AN4642,AN4870 and AN4912, which all assume MCAT is already running.&lt;/P&gt;&lt;P&gt;So, where is it?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Feb 2021 19:29:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Where-is-MCAT/m-p/1229518#M571</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2021-02-10T19:29:21Z</dc:date>
    </item>
    <item>
      <title>Re: Where is MCAT?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Where-is-MCAT/m-p/1229709#M572</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/7714"&gt;@GaryOlmstead&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;MCAT is part of the SDK and can imported from packaged "demo apps". So here are the steps (the first one is just there to validate you got everything in your SDK):&lt;/P&gt;
&lt;P&gt;1. Generate SDK with Motor Control option selected (it will&amp;nbsp;automatically select FreeMASTER as well)&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Capture.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137008iB70BD44A8FBFADC7/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;2. Once the SDK is added to MCUXpresso IDE, import the project from SDK examples&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Capture4.PNG" style="width: 271px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137010i1ABAD014159A7835/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture4.PNG" alt="Capture4.PNG" /&gt;&lt;/span&gt;BLDC &amp;amp; PSM example projects can be found under "demo_apps" section&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Capture1.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137013iDCE1A405BA033E40/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture1.PNG" alt="Capture1.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;3. FreeMASTER project is located in motor_control&amp;nbsp;&lt;SPAN&gt;→ freemaster&amp;nbsp;→ bldc.pmp (or pmsm.pmp)&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Capture2.PNG" style="width: 158px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137012i6EA637D70BAC1E90/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture2.PNG" alt="Capture2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;4. You can launch "pmp" file directly from project explorer which will open it in FreeMASTER tool.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Capture3.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/137014i87B58CBC111C87C1/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture3.PNG" alt="Capture3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Kind regards,&lt;BR /&gt;Iulian&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 07:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Where-is-MCAT/m-p/1229709#M572</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2021-02-11T07:34:14Z</dc:date>
    </item>
    <item>
      <title>Re: Where is MCAT?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Where-is-MCAT/m-p/1229998#M573</link>
      <description>&lt;P&gt;Hi Iulian --&lt;/P&gt;&lt;P&gt;Got it!!&amp;nbsp; It works!!&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;P&gt;Gary Olmstead&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 11 Feb 2021 17:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Where-is-MCAT/m-p/1229998#M573</guid>
      <dc:creator>GaryOlmstead</dc:creator>
      <dc:date>2021-02-11T17:08:51Z</dc:date>
    </item>
  </channel>
</rss>