<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックVector VN1630A LIN Support</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Vector-VN1630A-LIN-Support/m-p/1226199#M557</link>
    <description>&lt;P&gt;I want to use freeMaster over lin communication, but it only supports nican. Can support device: vector vn1630A?&lt;/P&gt;</description>
    <pubDate>Thu, 04 Feb 2021 08:05:19 GMT</pubDate>
    <dc:creator>WattYao</dc:creator>
    <dc:date>2021-02-04T08:05:19Z</dc:date>
    <item>
      <title>Vector VN1630A LIN Support</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Vector-VN1630A-LIN-Support/m-p/1226199#M557</link>
      <description>&lt;P&gt;I want to use freeMaster over lin communication, but it only supports nican. Can support device: vector vn1630A?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 08:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Vector-VN1630A-LIN-Support/m-p/1226199#M557</guid>
      <dc:creator>WattYao</dc:creator>
      <dc:date>2021-02-04T08:05:19Z</dc:date>
    </item>
    <item>
      <title>Re: Vector VN1630A LIN Support</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Vector-VN1630A-LIN-Support/m-p/1226204#M558</link>
      <description>&lt;P&gt;Dear WattYao,&lt;/P&gt;
&lt;P&gt;yes, FreeMASTER-over-LIN is still a bit experimental feature as it needs pretty specific support on the target side (multi-frame transport layer, diag-class II or III). There were just few users interested in this solution so far, so the PC support has not evolved more than to a single NI USB-to-LIC device support.&lt;/P&gt;
&lt;P&gt;The situation with FreeMASTER-over-CAN is different. There are many users and wide support for different CAN hardware including Vector, HMS Ixxat, Kvaser and others.&lt;/P&gt;
&lt;P&gt;Can you tell more about your target application? Do you use NXP LIN communication stack? What is your target platform?&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 08:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Vector-VN1630A-LIN-Support/m-p/1226204#M558</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2021-02-04T08:16:41Z</dc:date>
    </item>
    <item>
      <title>Re: Vector VN1630A LIN Support</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Vector-VN1630A-LIN-Support/m-p/1226221#M559</link>
      <description>&lt;P&gt;The platform is MC9S12ZVM,&amp;nbsp;&lt;SPAN&gt;there will be no CAN transceiver in mass production, only LIN communication.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 08:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Vector-VN1630A-LIN-Support/m-p/1226221#M559</guid>
      <dc:creator>WattYao</dc:creator>
      <dc:date>2021-02-04T08:25:50Z</dc:date>
    </item>
  </channel>
</rss>