<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Freemaster 3.1 - example project with MCUXpresso in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-1-example-project-with-MCUXpresso/m-p/1223617#M548</link>
    <description>&lt;P&gt;Greetings!&lt;/P&gt;&lt;P&gt;Using FreeMaster 3.1 with the RT1010EVK and MCUXpresso.&amp;nbsp; In my SDK, I have download the FreeMaster example uart application, and it runs on my RT1010EVK board.&lt;/P&gt;&lt;P&gt;In FreeMaster, I can connect to the board through the "Connection Wizard" with the simple serial port.&amp;nbsp; Now, what can I "do" in FreeMaster?&amp;nbsp; Is there an example tutorial that shows how to view/add the cariables in the firmware to FreeMaster?&amp;nbsp; Is there a ready-made FreeMaster project that I can load with this SDK example?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 31 Jan 2021 18:42:13 GMT</pubDate>
    <dc:creator>rt54321</dc:creator>
    <dc:date>2021-01-31T18:42:13Z</dc:date>
    <item>
      <title>Freemaster 3.1 - example project with MCUXpresso</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-1-example-project-with-MCUXpresso/m-p/1223617#M548</link>
      <description>&lt;P&gt;Greetings!&lt;/P&gt;&lt;P&gt;Using FreeMaster 3.1 with the RT1010EVK and MCUXpresso.&amp;nbsp; In my SDK, I have download the FreeMaster example uart application, and it runs on my RT1010EVK board.&lt;/P&gt;&lt;P&gt;In FreeMaster, I can connect to the board through the "Connection Wizard" with the simple serial port.&amp;nbsp; Now, what can I "do" in FreeMaster?&amp;nbsp; Is there an example tutorial that shows how to view/add the cariables in the firmware to FreeMaster?&amp;nbsp; Is there a ready-made FreeMaster project that I can load with this SDK example?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 31 Jan 2021 18:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-1-example-project-with-MCUXpresso/m-p/1223617#M548</guid>
      <dc:creator>rt54321</dc:creator>
      <dc:date>2021-01-31T18:42:13Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.1 - example project with MCUXpresso</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-1-example-project-with-MCUXpresso/m-p/1223914#M549</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/182943"&gt;@rt54321&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;In the root folder of your project you will find a corresponding FreeMASTER project (`.pmp` file).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Capture.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/136203i108940E573DD624E/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture.PNG" alt="Capture.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Capture.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There is a basic example on FreeMASTER usage available in this &lt;A href="https://community.nxp.com/t5/FreeMASTER-Knowledge-Base/Connecting-to-the-Board/ta-p/1122819" target="_self"&gt;article&lt;/A&gt; (video). A more extensive example about FreeMASTER features can be found&amp;nbsp;&lt;A href="https://www.nxp.com/design/training/get-to-know-the-freemaster-runtime-debugging-tool:TIP-GET-TO-KNOW-FREEMASTER-RUNTIME-DEBUGGING-TOOL" target="_self"&gt;here&lt;/A&gt; (webinar VOD).&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Iulian&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 08:37:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-1-example-project-with-MCUXpresso/m-p/1223914#M549</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2021-02-01T08:37:13Z</dc:date>
    </item>
  </channel>
</rss>