<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックScope Trigger Options</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Scope-Trigger-Options/m-p/1208408#M518</link>
    <description>&lt;P&gt;I see no &lt;STRONG&gt;Trigger&lt;/STRONG&gt; options in &lt;STRONG&gt;Scope&lt;/STRONG&gt; as e.g. in &lt;STRONG&gt;Segger J-Scope&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Is it possible to add it?&lt;/P&gt;&lt;P&gt;Technically it could not be a problem.&lt;/P&gt;</description>
    <pubDate>Thu, 07 Jan 2021 16:02:21 GMT</pubDate>
    <dc:creator>kabron1</dc:creator>
    <dc:date>2021-01-07T16:02:21Z</dc:date>
    <item>
      <title>Scope Trigger Options</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Scope-Trigger-Options/m-p/1208408#M518</link>
      <description>&lt;P&gt;I see no &lt;STRONG&gt;Trigger&lt;/STRONG&gt; options in &lt;STRONG&gt;Scope&lt;/STRONG&gt; as e.g. in &lt;STRONG&gt;Segger J-Scope&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;Is it possible to add it?&lt;/P&gt;&lt;P&gt;Technically it could not be a problem.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 16:02:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Scope-Trigger-Options/m-p/1208408#M518</guid>
      <dc:creator>kabron1</dc:creator>
      <dc:date>2021-01-07T16:02:21Z</dc:date>
    </item>
    <item>
      <title>Re: Scope Trigger Options</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Scope-Trigger-Options/m-p/1208812#M520</link>
      <description>&lt;P&gt;Dear Vladimir,&lt;/P&gt;
&lt;P&gt;the oscilloscope values are all processed on the PC so adding a condition which would hold the data until a trigger comes is definitely technically possible. And it is actually very good idea, I will add it to the feature request backlog for future versions.&lt;/P&gt;
&lt;P&gt;Currently, the triggering is only possible in the Recorder, which runs as a part of FreeMASTER driver on the microcontroller side. You would need to connect using Serial, CAN or packet-driven JTAG/BDM (PD-BDM) option to make use of the Recorder feature.&lt;/P&gt;
&lt;P&gt;Thank you,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 08:31:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Scope-Trigger-Options/m-p/1208812#M520</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2021-01-08T08:31:23Z</dc:date>
    </item>
  </channel>
</rss>