<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: Can freemaster connect target device via Ethernet TCP?</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Can-freemaster-connect-target-device-via-Ethernet-TCP/m-p/1170221#M447</link>
    <description>&lt;P&gt;Thanks very much, I will try another way.&lt;/P&gt;</description>
    <pubDate>Tue, 20 Oct 2020 08:51:50 GMT</pubDate>
    <dc:creator>Sharingan666</dc:creator>
    <dc:date>2020-10-20T08:51:50Z</dc:date>
    <item>
      <title>Can freemaster connect target device via Ethernet TCP?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Can-freemaster-connect-target-device-via-Ethernet-TCP/m-p/1169943#M445</link>
      <description>&lt;P&gt;Hi,I want to connet my target device via Ethernet port, does freemaster support this function? I found TCP communcation configuraton in "Option" dialog, but can not find any&amp;nbsp;introduction in freemaster softtware user guide. Can I use this communcation function?&lt;/P&gt;&lt;P&gt;Thinks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="屏幕截图 2020-10-20 100057.png" style="width: 684px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/127796i8A638AC0079CAE29/image-size/large?v=v2&amp;amp;px=999" role="button" title="屏幕截图 2020-10-20 100057.png" alt="屏幕截图 2020-10-20 100057.png" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 02:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Can-freemaster-connect-target-device-via-Ethernet-TCP/m-p/1169943#M445</guid>
      <dc:creator>Sharingan666</dc:creator>
      <dc:date>2020-10-20T02:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: Can freemaster connect target device via Ethernet TCP?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Can-freemaster-connect-target-device-via-Ethernet-TCP/m-p/1170097#M446</link>
      <description>&lt;P&gt;Dear user,&lt;/P&gt;
&lt;P&gt;direct TCP or UDP communication is not yet available in FreeMASTER. We have it in our plans, but the release is not scheduled for this year.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You are correct that there is an experimental version of the TCP plug in in the list, but this is currently not usable.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 06:43:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Can-freemaster-connect-target-device-via-Ethernet-TCP/m-p/1170097#M446</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-10-20T06:43:21Z</dc:date>
    </item>
    <item>
      <title>Re: Can freemaster connect target device via Ethernet TCP?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Can-freemaster-connect-target-device-via-Ethernet-TCP/m-p/1170221#M447</link>
      <description>&lt;P&gt;Thanks very much, I will try another way.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 08:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Can-freemaster-connect-target-device-via-Ethernet-TCP/m-p/1170221#M447</guid>
      <dc:creator>Sharingan666</dc:creator>
      <dc:date>2020-10-20T08:51:50Z</dc:date>
    </item>
  </channel>
</rss>