<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 TWR-58F220M Freemaster Connection Problem</title>
    <link>https://community.nxp.com/t5/FreeMASTER/TWR-58F220M-Freemaster-Connection-Problem/m-p/1149270#M426</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have some problems with freemaster connection. I am using tower board system TWR-KV58F220M and TWR-MC-LV3PH. Also I am using J-link.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, I can program the board successful via Keil. Motor is spinnig. But when I try to Freemaster, I have failed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Open Freemaster 3.0 and open the ready project 'bldc_ref_sol.pmp'. And press to GO button then I have received a message that "Could not open the communication port". Also error code is 0x80000101. The other thing is opening message is 'missing symbol definitions' that I attached.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="missing_symbols.PNG" style="width: 518px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124427i758086193EDC25DD/image-size/large?v=v2&amp;amp;px=999" role="button" title="missing_symbols.PNG" alt="missing_symbols.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My comport arrangements and baudrate are true.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I followed this steps for solution:&lt;/P&gt;&lt;P&gt;Tools -&amp;gt; Connection Wizard -&amp;gt; Connect through a debugger probe or on-board debugger interface -&amp;gt; J-Link or J-Trace interface from segger microcontroller -&amp;gt; Direct Access (And I have nothing, I connot end this process)&lt;/P&gt;&lt;P&gt;Also followed this video in &lt;A href="https://www.nxp.com/design/designs/kv-series-3-phase-brushless-dc-motor-control-reference-design:BRUSHLESS-DC-MOTOR-CONTROL" target="_self"&gt;link&lt;/A&gt; but I cannot solve the problem again. Still my App ID is offline.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AppID_Off.PNG" style="width: 847px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124428iBB35C74B8A37736C/image-size/large?v=v2&amp;amp;px=999" role="button" title="AppID_Off.PNG" alt="AppID_Off.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;</description>
    <pubDate>Sat, 05 Sep 2020 20:25:47 GMT</pubDate>
    <dc:creator>alihanc_caliska</dc:creator>
    <dc:date>2020-09-05T20:25:47Z</dc:date>
    <item>
      <title>TWR-58F220M Freemaster Connection Problem</title>
      <link>https://community.nxp.com/t5/FreeMASTER/TWR-58F220M-Freemaster-Connection-Problem/m-p/1149270#M426</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have some problems with freemaster connection. I am using tower board system TWR-KV58F220M and TWR-MC-LV3PH. Also I am using J-link.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, I can program the board successful via Keil. Motor is spinnig. But when I try to Freemaster, I have failed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Open Freemaster 3.0 and open the ready project 'bldc_ref_sol.pmp'. And press to GO button then I have received a message that "Could not open the communication port". Also error code is 0x80000101. The other thing is opening message is 'missing symbol definitions' that I attached.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="missing_symbols.PNG" style="width: 518px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124427i758086193EDC25DD/image-size/large?v=v2&amp;amp;px=999" role="button" title="missing_symbols.PNG" alt="missing_symbols.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;My comport arrangements and baudrate are true.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I followed this steps for solution:&lt;/P&gt;&lt;P&gt;Tools -&amp;gt; Connection Wizard -&amp;gt; Connect through a debugger probe or on-board debugger interface -&amp;gt; J-Link or J-Trace interface from segger microcontroller -&amp;gt; Direct Access (And I have nothing, I connot end this process)&lt;/P&gt;&lt;P&gt;Also followed this video in &lt;A href="https://www.nxp.com/design/designs/kv-series-3-phase-brushless-dc-motor-control-reference-design:BRUSHLESS-DC-MOTOR-CONTROL" target="_self"&gt;link&lt;/A&gt; but I cannot solve the problem again. Still my App ID is offline.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="AppID_Off.PNG" style="width: 847px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/124428iBB35C74B8A37736C/image-size/large?v=v2&amp;amp;px=999" role="button" title="AppID_Off.PNG" alt="AppID_Off.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Sat, 05 Sep 2020 20:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/TWR-58F220M-Freemaster-Connection-Problem/m-p/1149270#M426</guid>
      <dc:creator>alihanc_caliska</dc:creator>
      <dc:date>2020-09-05T20:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-58F220M Freemaster Connection Problem</title>
      <link>https://community.nxp.com/t5/FreeMASTER/TWR-58F220M-Freemaster-Connection-Problem/m-p/1156231#M431</link>
      <description>&lt;P&gt;Dear user,&lt;/P&gt;
&lt;P&gt;I cannot comment on this particular KV58 application, but let's first try some general hints:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;When connecting over the debugging probe, please make sure your existing debugger session is closed so the debugger does not keep the J-Link device occupied.&lt;/LI&gt;
&lt;LI&gt;When detaching the debugger connection, sometimes the target application stops. Make sure it is running by resetting the hardware board.&lt;/LI&gt;
&lt;LI&gt;In the JLink Communication plug-in settings, don't forget to specify Cortex-M4/M7 or even select the KV58 from the CPU list.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;If none of the hints help, please send me a screenshot of your plug-in settings.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 11:39:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/TWR-58F220M-Freemaster-Connection-Problem/m-p/1156231#M431</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-09-21T11:39:36Z</dc:date>
    </item>
  </channel>
</rss>