<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FreeMASTER 3.0 no Plug-in module in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-3-0-no-Plug-in-module/m-p/986544#M38</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Dariusz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there must be something wrong with the FreeMASTER installation on your computer. The plug-ins are system DLLs which are registered in system registry during installer process. Please&amp;nbsp;try to re-install the FreeMASTER 3.0&amp;nbsp;and make sure the installer is run with&amp;nbsp;administrator privileges.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically, the installation process is the same as running the&amp;nbsp;&lt;EM&gt;"c:\NXP\FreeMASTER 3.0\FreeMASTER\register.bat"&amp;nbsp;&lt;/EM&gt; with&amp;nbsp;administrator rights. If re-installation does not help, can you try to run this file manually in a cmd console window (started as administrator) and see what it prints?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Dec 2019 15:35:35 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2019-12-16T15:35:35Z</dc:date>
    <item>
      <title>FreeMASTER 3.0 no Plug-in module</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-3-0-no-Plug-in-module/m-p/986543#M37</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon, ladies and gentlemen,&lt;BR /&gt;I bought a TWR-KM34Z75M development board and try to realize a 1-phase energy measurement with it.&lt;BR /&gt;My programming development environment (IDE) is the IAR EW with version 8.40.2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded sample programs for this (KM34Z75_EXAMPLES.exe.zip)&lt;BR /&gt;in this archive under KM34Z75_EXAMPLES\build\iar_7_40\projects\_1phmeter_example you can find a sample project about my topic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also a PDF_file is provided for explanation (readme.pdf).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are the settings shown in the different programs you should do. Since it is an example program for the development environment IDE IAR EW created, I do not have to change there.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But the settings for the second program for visualization (FreeMASTER 3.0) I have to do completely by myself.&lt;/P&gt;&lt;P&gt;It fails however ready at the setting of the interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Next you will see an excerpt from the readme.pdf file page 5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96803i469F099F82B41794/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and here an excerpt from my program:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96827iCC1843B9CE96FDE2/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I can't select a plug-in module and I don't know why.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could someone help me out in this matter ?&lt;/P&gt;&lt;P&gt;Thanks in beforehand.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2019 15:27:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-3-0-no-Plug-in-module/m-p/986543#M37</guid>
      <dc:creator>dariusz_hurek</dc:creator>
      <dc:date>2019-12-16T15:27:42Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER 3.0 no Plug-in module</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-3-0-no-Plug-in-module/m-p/986544#M38</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Dariusz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there must be something wrong with the FreeMASTER installation on your computer. The plug-ins are system DLLs which are registered in system registry during installer process. Please&amp;nbsp;try to re-install the FreeMASTER 3.0&amp;nbsp;and make sure the installer is run with&amp;nbsp;administrator privileges.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Basically, the installation process is the same as running the&amp;nbsp;&lt;EM&gt;"c:\NXP\FreeMASTER 3.0\FreeMASTER\register.bat"&amp;nbsp;&lt;/EM&gt; with&amp;nbsp;administrator rights. If re-installation does not help, can you try to run this file manually in a cmd console window (started as administrator) and see what it prints?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2019 15:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-3-0-no-Plug-in-module/m-p/986544#M38</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2019-12-16T15:35:35Z</dc:date>
    </item>
  </channel>
</rss>