<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックBit mask does not work with 64bit variable</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Bit-mask-does-not-work-with-64bit-variable/m-p/1079110#M327</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If we configure in Freemaster 3.0.3.6 a bitmask to a 8byte (64bit) variable, it doesen't work. The bitmask has no effect to the value.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/114966iF52C3A913E8EE309/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jul 2020 11:19:00 GMT</pubDate>
    <dc:creator>martinrieser</dc:creator>
    <dc:date>2020-07-08T11:19:00Z</dc:date>
    <item>
      <title>Bit mask does not work with 64bit variable</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Bit-mask-does-not-work-with-64bit-variable/m-p/1079110#M327</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If we configure in Freemaster 3.0.3.6 a bitmask to a 8byte (64bit) variable, it doesen't work. The bitmask has no effect to the value.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/114966iF52C3A913E8EE309/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2020 11:19:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Bit-mask-does-not-work-with-64bit-variable/m-p/1079110#M327</guid>
      <dc:creator>martinrieser</dc:creator>
      <dc:date>2020-07-08T11:19:00Z</dc:date>
    </item>
    <item>
      <title>Re: Bit mask does not work with 64bit variable</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Bit-mask-does-not-work-with-64bit-variable/m-p/1079111#M328</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Martin,&lt;/P&gt;&lt;P&gt;thank you for reporting this.&amp;nbsp;I confirm two issues - will address it in the next release:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;the mask value is limited to 32 bits only&lt;/LI&gt;&lt;LI&gt;masked-write of&amp;nbsp;64bit variable&amp;nbsp;is rejected&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading a 64bit variable, shifting it and masking with a&amp;nbsp;mask value limited to 32bits should work without issues.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a workaround, you can define&amp;nbsp;two helper 4-byte variables with an addresses "symbol" and "symbol+4" - and access them separately.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jul 2020 08:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Bit-mask-does-not-work-with-64bit-variable/m-p/1079111#M328</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-07-10T08:30:57Z</dc:date>
    </item>
  </channel>
</rss>