<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: FreeMASTER source codes</title>
    <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-source-codes/m-p/1078746#M326</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Stepan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the source code of FreeMASTER serial and CAN communication driver is available&amp;nbsp;in the &lt;A href="https://mcuxpresso.nxp.com/en"&gt;MCUXpresso SDK&lt;/A&gt;. The source code is the same for all MCUs supported&amp;nbsp;by the SDK, so just pick any of the supported devices&amp;nbsp;or boards (e.g. FRDM-K64F) and&amp;nbsp;add the FreeMASTER&amp;nbsp; middleware component. The sources will be located in middleware/freemaster directory in the generated SDK ZIP package.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you ask about sources of the FreeMASTER desktop applications, then the answer is no. The sources are not publicly available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 May 2020 07:29:03 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2020-05-13T07:29:03Z</dc:date>
    <item>
      <title>FreeMASTER source codes</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-source-codes/m-p/1078745#M325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;please can anybody tell me whether the source codes for the FreeMASTER software are available for download? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 18:28:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-source-codes/m-p/1078745#M325</guid>
      <dc:creator>stepan_podhorsk</dc:creator>
      <dc:date>2020-05-12T18:28:58Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER source codes</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-source-codes/m-p/1078746#M326</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Stepan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the source code of FreeMASTER serial and CAN communication driver is available&amp;nbsp;in the &lt;A href="https://mcuxpresso.nxp.com/en"&gt;MCUXpresso SDK&lt;/A&gt;. The source code is the same for all MCUs supported&amp;nbsp;by the SDK, so just pick any of the supported devices&amp;nbsp;or boards (e.g. FRDM-K64F) and&amp;nbsp;add the FreeMASTER&amp;nbsp; middleware component. The sources will be located in middleware/freemaster directory in the generated SDK ZIP package.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you ask about sources of the FreeMASTER desktop applications, then the answer is no. The sources are not publicly available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2020 07:29:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-source-codes/m-p/1078746#M326</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-05-13T07:29:03Z</dc:date>
    </item>
  </channel>
</rss>