<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 Robot monitoring idea using #freemasterdash</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Robot-monitoring-idea-using-freemasterdash/m-p/1077514#M323</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got a current project where I need to monitor the state of a number of industrial robots such as is the e-Stop has been triggered. I also need to stop and start them remotely.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was initially going to host a very simple UI on an FRDM-K64F, but FreeMASTER seems like a good fit for creating a nicer UI for this process - including status indicators and controls. I've spent many years as a web developer so will probably use custom code rather than relying on 3rd party widgets.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 May 2020 15:42:01 GMT</pubDate>
    <dc:creator>fred27murphy</dc:creator>
    <dc:date>2020-05-26T15:42:01Z</dc:date>
    <item>
      <title>Robot monitoring idea using #freemasterdash</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Robot-monitoring-idea-using-freemasterdash/m-p/1077514#M323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got a current project where I need to monitor the state of a number of industrial robots such as is the e-Stop has been triggered. I also need to stop and start them remotely.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was initially going to host a very simple UI on an FRDM-K64F, but FreeMASTER seems like a good fit for creating a nicer UI for this process - including status indicators and controls. I've spent many years as a web developer so will probably use custom code rather than relying on 3rd party widgets.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 15:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Robot-monitoring-idea-using-freemasterdash/m-p/1077514#M323</guid>
      <dc:creator>fred27murphy</dc:creator>
      <dc:date>2020-05-26T15:42:01Z</dc:date>
    </item>
    <item>
      <title>Re: Robot monitoring idea using #freemasterdash</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Robot-monitoring-idea-using-freemasterdash/m-p/1077515#M324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Fred,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this is a great plan. I can't wait to see the result. In case of any problem with JSON-RPC API or FreeMASTER interfacing, don't hesitate to submit a question to this forum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 06:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Robot-monitoring-idea-using-freemasterdash/m-p/1077515#M324</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-05-27T06:50:23Z</dc:date>
    </item>
  </channel>
</rss>