<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 Freemaster with RT1010 (AN12591)</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986403#M32</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to set up FRDM-MC-LVPMSM with RT1010 as in AN12591. I am using&amp;nbsp;FRDM-MC-LVMTR motor and connected three phase lines only. I compiled the sample program, downloaded it to the board. Freemaster seems to be connected to the board. I can not make the motor run. For example, I can not change the application switch variable to ON. Is there anything I am missing? I haven't connect the encoder pins to the motor. How should I have to connect it? Any schematic available?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97033iC1F2906F5CEEE72E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Dec 2019 18:59:59 GMT</pubDate>
    <dc:creator>ykim</dc:creator>
    <dc:date>2019-12-17T18:59:59Z</dc:date>
    <item>
      <title>Freemaster with RT1010 (AN12591)</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986403#M32</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried to set up FRDM-MC-LVPMSM with RT1010 as in AN12591. I am using&amp;nbsp;FRDM-MC-LVMTR motor and connected three phase lines only. I compiled the sample program, downloaded it to the board. Freemaster seems to be connected to the board. I can not make the motor run. For example, I can not change the application switch variable to ON. Is there anything I am missing? I haven't connect the encoder pins to the motor. How should I have to connect it? Any schematic available?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/97033iC1F2906F5CEEE72E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2019 18:59:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986403#M32</guid>
      <dc:creator>ykim</dc:creator>
      <dc:date>2019-12-17T18:59:59Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster with RT1010 (AN12591)</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986404#M33</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kim,&lt;/P&gt;&lt;P&gt;For compatibility with LCD display, the RT1010-EVK hardware board must be reworked following &lt;STRONG&gt;chapter 4.1.2 and Figure 6,7 in&lt;/STRONG&gt; AN12591.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98453i33A34AD3DACC8039/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2019 02:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986404#M33</guid>
      <dc:creator>wesson_ding</dc:creator>
      <dc:date>2019-12-20T02:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster with RT1010 (AN12591)</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986405#M34</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;RT1010-EVK schematic and be downloaded from this link:&lt;/P&gt;&lt;P&gt;&lt;A class="jivelink11" href="https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/i.mx-rt1010-evaluation-kit:MIMXRT1010-EVK" title="https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/i.mx-rt1010-evaluation-kit:MIMXRT1010-EVK"&gt;https://www.nxp.com/design/development-boards/i.mx-evaluation-and-development-boards/i.mx-rt1010-evaluation-kit:MIMXRT1010-EVK&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2019 02:42:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986405#M34</guid>
      <dc:creator>wesson_ding</dc:creator>
      <dc:date>2019-12-20T02:42:10Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster with RT1010 (AN12591)</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986406#M35</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was trying without the lcd panel. I can re-try after re-work the board. However, shouldn't this free master application run without LCD ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2019 06:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986406#M35</guid>
      <dc:creator>ykim</dc:creator>
      <dc:date>2019-12-23T06:50:35Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster with RT1010 (AN12591)</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986407#M36</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. In order to be compatible with LCD, some ADC sampling channels and PWM pins must be changed, even if LCD is not used, rework is required&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; If you want to run the demo with freemaster, pls follow the steps in AN12591.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/100331i6DFB4E6F8D99EB65/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Dec 2019 07:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-with-RT1010-AN12591/m-p/986407#M36</guid>
      <dc:creator>wesson_ding</dc:creator>
      <dc:date>2019-12-31T07:10:05Z</dc:date>
    </item>
  </channel>
</rss>