<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: PD-BDM with iSYSTEM winIDEA won't work</title>
    <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074414#M315</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Michal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the FreeMASTER variable definition as uint16:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107902i013B3271CF40CC57/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And this the definition of the same variable as uint32:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107925i996CA4E31240EF5A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the FreeMASTER watch:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107962i4BB4EE970C2A159E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And this is winIDEA debugger:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108098i455BFC8021B3A7E8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Everything looks consistent though. I am available to do further checks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 May 2020 07:12:25 GMT</pubDate>
    <dc:creator>lucabarbiero</dc:creator>
    <dc:date>2020-05-27T07:12:25Z</dc:date>
    <item>
      <title>PD-BDM with iSYSTEM winIDEA won't work</title>
      <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074410#M311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I work with FreeMASTER 2.5 and my debugger environment is winIDEA 9.17.100 from iSYSTEM. I can connect to the target with direct access to the memory, but I fail to do so using the PD-BDM protocol (which I need because I want to use the FreeMASTER recorder feature).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I compiled the FreeMASTER communication driver on the target with the appropriate option:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define &lt;SPAN style="color: #ff0000;"&gt;FMSTR_USE_PDBDM 1&lt;/SPAN&gt; /* To select Packet Driven BDM communication interface (optional) */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I know the address of the packet buffer:&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107850i63D36206E756178B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the FreeMASTER plugin I can see that the connection with winIDEA is successful:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107928iEA82B1FC57EBD9E5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But it fails to find the packet buffer at the specified address (and the automatic search runs but cannot find it as well):&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108214iD9BDF0CAD3CE334D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why it does not work? :smileysad:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 08:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074410#M311</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2020-05-26T08:19:27Z</dc:date>
    </item>
    <item>
      <title>Re: PD-BDM with iSYSTEM winIDEA won't work</title>
      <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074411#M312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Luca,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can you try installing the latest FreeMASTER version 3.0 (3.0.2)?&amp;nbsp;Installing this version will register a new PD-BDM plug-in version in system. You will be able to use it&amp;nbsp;also&amp;nbsp;from&amp;nbsp;both 2.5 and 3.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There were few compatibility issues solved in PD-BDM since the version released with FreeMASTER 2.5, so I believe&amp;nbsp;this operation will help. Let me know if not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 12:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074411#M312</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-05-26T12:48:27Z</dc:date>
    </item>
    <item>
      <title>Re: PD-BDM with iSYSTEM winIDEA won't work</title>
      <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074412#M313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Michal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your prompt reply. I installed FreeMASTER 3.0 but the problem persists, using either &lt;SPAN&gt;FreeMASTER&amp;nbsp;&lt;/SPAN&gt;3.0 or 2.5 (I understand that the plugin is the same but I tried with both versions anyway). Here is a screenshot:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107896i95246C87C87BCB80/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will recognize from it that this is the new plugin (the GUI is different). Still no success. I Inserted the address and I also did a search just in case. So the problem is still there. Note that I am using a recent version of winIDEA&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;9.17.100 (released 9/2019). Maybe when you tested the plugin you used the previous version 9.17.39? I can't say if the problem could be here, recall that I can connect with direct memory access (so I can confirm that debugger and target are reachable by FreeMASTER). The issue is when trying to connect with PD-BDM.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Luca&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 May 2020 14:36:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074412#M313</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2020-05-26T14:36:55Z</dc:date>
    </item>
    <item>
      <title>Re: PD-BDM with iSYSTEM winIDEA won't work</title>
      <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074413#M314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Luca,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can you please create a FreeMASTER variable (2-byte unsigned int) at the expected address of the PD-BDM buffer (0x40001b00)? And please display its value in a variable watch and send it to me here. Then update the variable to 4 byte size and send me the value too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect we have a compatibility issue of PD-BDM operation and big-endian parts. I will test also locally.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 06:45:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074413#M314</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-05-27T06:45:33Z</dc:date>
    </item>
    <item>
      <title>Re: PD-BDM with iSYSTEM winIDEA won't work</title>
      <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074414#M315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Michal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the FreeMASTER variable definition as uint16:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107902i013B3271CF40CC57/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And this the definition of the same variable as uint32:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107925i996CA4E31240EF5A/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the FreeMASTER watch:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107962i4BB4EE970C2A159E/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And this is winIDEA debugger:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108098i455BFC8021B3A7E8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Everything looks consistent though. I am available to do further checks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 07:12:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074414#M315</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2020-05-27T07:12:25Z</dc:date>
    </item>
    <item>
      <title>Re: PD-BDM with iSYSTEM winIDEA won't work</title>
      <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074415#M316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much. Let me prepare a fix for you to test. It should be available by tomorrow. Can you contact me directly on this &lt;A href="mailto:michal.hanak@nxp.com"&gt;email&lt;/A&gt;?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 07:21:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074415#M316</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-05-27T07:21:48Z</dc:date>
    </item>
    <item>
      <title>Re: PD-BDM with iSYSTEM winIDEA won't work</title>
      <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074416#M317</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Michal, thanks for the patch you sent me. Now it works!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 13:44:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074416#M317</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2020-05-27T13:44:29Z</dc:date>
    </item>
    <item>
      <title>Re: PD-BDM with iSYSTEM winIDEA won't work</title>
      <link>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074417#M318</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Luca, thanks for your cooperation. The fix will officially appear in FreeMASTER 3.0.3 in June 2020.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If observing a performance issues with PD-BDM, please note that you can&amp;nbsp;select Direct BDM Memory Read and Write&amp;nbsp;so the packet-driven protocol is not used for such basic operations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 May 2020 13:50:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/PD-BDM-with-iSYSTEM-winIDEA-won-t-work/m-p/1074417#M318</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-05-27T13:50:38Z</dc:date>
    </item>
  </channel>
</rss>