<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックReasons FreeMASTER wouldn't detect PEAK PCAN connections?</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Reasons-FreeMASTER-wouldn-t-detect-PEAK-PCAN-connections/m-p/1069372#M301</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Setup&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;NXP MPC5777C&lt;/P&gt;&lt;P&gt;FreeMASTER 3.0.3.6 (comm.protocol v3+, v4)&lt;/P&gt;&lt;P&gt;(1x) 120 Ohm termination resistor on my PEAK PCAN APIv4.1.0.96 (USB/CAN) connector (enough to terminate otherwise)&lt;/P&gt;&lt;P&gt;(See the attached .png for the error encountered.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot seem to get FreeMASTER connected via CAN bus, though my freemaster_cfg.h-file is configured appropriately and I can Rx messages appropriately via CAN bus with my board's hardware.&amp;nbsp; Are there any reasons FreeMASTER wouldn't detect PEAK PCAN connections?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Aug 2020 20:56:35 GMT</pubDate>
    <dc:creator>max_perko</dc:creator>
    <dc:date>2020-08-26T20:56:35Z</dc:date>
    <item>
      <title>Reasons FreeMASTER wouldn't detect PEAK PCAN connections?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Reasons-FreeMASTER-wouldn-t-detect-PEAK-PCAN-connections/m-p/1069372#M301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Setup&lt;/STRONG&gt;:&lt;/P&gt;&lt;P&gt;NXP MPC5777C&lt;/P&gt;&lt;P&gt;FreeMASTER 3.0.3.6 (comm.protocol v3+, v4)&lt;/P&gt;&lt;P&gt;(1x) 120 Ohm termination resistor on my PEAK PCAN APIv4.1.0.96 (USB/CAN) connector (enough to terminate otherwise)&lt;/P&gt;&lt;P&gt;(See the attached .png for the error encountered.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot seem to get FreeMASTER connected via CAN bus, though my freemaster_cfg.h-file is configured appropriately and I can Rx messages appropriately via CAN bus with my board's hardware.&amp;nbsp; Are there any reasons FreeMASTER wouldn't detect PEAK PCAN connections?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Aug 2020 20:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Reasons-FreeMASTER-wouldn-t-detect-PEAK-PCAN-connections/m-p/1069372#M301</guid>
      <dc:creator>max_perko</dc:creator>
      <dc:date>2020-08-26T20:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: Reasons FreeMASTER wouldn't detect PEAK PCAN connections?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Reasons-FreeMASTER-wouldn-t-detect-PEAK-PCAN-connections/m-p/1069373#M302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Max,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it seems there is something wrong with the Windows PEAK driver. FreeMASTER cannot&amp;nbsp;detect the PEAK device connected&amp;nbsp;to the USB port. You need to see a valid "CAN Channel" name in the setup dialog. The word&amp;nbsp;"Unknown" means the device has not been detected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see your driver/API version is 4.1.0.96. When I did my testing, the version I got was 4.4.0.288 (that was January 2020).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Perhaps it could help to update the PEAK Windows drivers (especially the PCANBasic.dll) to the latest version and try again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2020 06:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Reasons-FreeMASTER-wouldn-t-detect-PEAK-PCAN-connections/m-p/1069373#M302</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2020-08-27T06:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: Reasons FreeMASTER wouldn't detect PEAK PCAN connections?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Reasons-FreeMASTER-wouldn-t-detect-PEAK-PCAN-connections/m-p/1069374#M303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thakks Michael&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thats a great idea.&amp;nbsp; I think It also makes sense to sanity check the CAN pins being used and memory map area defined for that particular CAN bus in the FREEMASTE confgi header file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Aug 2020 15:05:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Reasons-FreeMASTER-wouldn-t-detect-PEAK-PCAN-connections/m-p/1069374#M303</guid>
      <dc:creator>Daniel_Wax</dc:creator>
      <dc:date>2020-08-27T15:05:34Z</dc:date>
    </item>
  </channel>
</rss>