<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Application-Command-issue-in-examples-freemaster-examples-fmstr/m-p/2416528#M2247</link>
    <description>&lt;P&gt;Dear All&lt;/P&gt;&lt;P&gt;Downloaded sdk.sdk_2.x_lpcxpresso54114 with only FreeMASTER examples. It works correctly in any aspect apart the Application Command section where I find strange behavior&lt;/P&gt;&lt;P&gt;More details has been posted in github here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10" target="_blank"&gt;https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;Paolo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 27 Sep 2026 10:50:05 GMT</pubDate>
    <dc:creator>pberna67</dc:creator>
    <dc:date>2026-09-27T10:50:05Z</dc:date>
    <item>
      <title>Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Application-Command-issue-in-examples-freemaster-examples-fmstr/m-p/2416528#M2247</link>
      <description>&lt;P&gt;Dear All&lt;/P&gt;&lt;P&gt;Downloaded sdk.sdk_2.x_lpcxpresso54114 with only FreeMASTER examples. It works correctly in any aspect apart the Application Command section where I find strange behavior&lt;/P&gt;&lt;P&gt;More details has been posted in github here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10" target="_blank"&gt;https://github.com/nxp-mcuxpresso/mcuxsdk-examples/issues/10&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;Paolo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 27 Sep 2026 10:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Application-Command-issue-in-examples-freemaster-examples-fmstr/m-p/2416528#M2247</guid>
      <dc:creator>pberna67</dc:creator>
      <dc:date>2026-09-27T10:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: Application Command issue in 'examples/freemaster_examples/fmstr_example_pdbdm</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Application-Command-issue-in-examples-freemaster-examples-fmstr/m-p/2416988#M2248</link>
      <description>&lt;P&gt;Hello, if I understand the issue correctly, you do not see a reason why command 0x10 returns code 16 in the example application.&lt;/P&gt;
&lt;P&gt;The command 0x10 is registered for a callback function:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MichalH_0-1790669419958.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396998i4B4FABC8A6AD0CB5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MichalH_0-1790669419958.png" alt="MichalH_0-1790669419958.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;So the function "my_appcmd_handler" gets called automatically when FreeMASTER probes the command execution.&amp;nbsp; The example code of this callback is quite trivial:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MichalH_1-1790669515160.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396999i1092279E3D133C93/image-size/large?v=v2&amp;amp;px=999" role="button" title="MichalH_1-1790669515160.png" alt="MichalH_1-1790669515160.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Which is the reason you get the return code 16 (=0x10) as answer.&lt;/P&gt;
&lt;P&gt;I also confirm there is an issue in FreeMASTER with displaying a message for unknown responses as you reported for app.command with Id 0x02. The response 0xcd should be reported as "unknown response" but generates no message at all.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Sep 2026 08:14:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Application-Command-issue-in-examples-freemaster-examples-fmstr/m-p/2416988#M2248</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2026-09-29T08:14:10Z</dc:date>
    </item>
  </channel>
</rss>