<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRemote access to FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Remote-access-to-FreeMASTER/m-p/2415067#M2236</link>
    <description>&lt;P&gt;Dear All&lt;BR /&gt;&lt;BR /&gt;I would to access to FreeMaster running in a PC an connected to a target (LPC1766) via Jlink troughs a second PC connected in the same local network . Even if the connection to the local PC via e browser (Any),&amp;nbsp; using the simple example attached, works correctly, if move all files (attached) in a different PC, and finally I open the Test.htm in the remote browser, variable read don't work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Respect the original NXP example where it indicated local-host, now the address is changed and it always point to the PC where FreeMASTER runs.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pberna67_0-1790032198582.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396633i7DC931A7515F8A0E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pberna67_0-1790032198582.png" alt="pberna67_0-1790032198582.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any idea of the reason of this problem ?&lt;BR /&gt;&lt;BR /&gt;Is it possible to create a Windows App Form in a remote PC that is able to connect (as a DCOM Client ??, don't know) to the FreeMASTER of the "local" PC where FreeMASTER (DCOM Server??) runs and it is connected to the target via Jlink emulator?,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;1) What is the configuration of FreeMASTER of the local PC ?&lt;BR /&gt;2) How do I access via Visual Basic .NET&amp;nbsp; Form APP to the local PC from (where FreeMASTER runs) the Remote PC ?&lt;BR /&gt;&lt;BR /&gt;The reason of these questions is because my develop PC where Microsoft Visual Studio. .NET runs is not the same machine where FreeMASTER and the target board (LPC1766) are,&lt;/P&gt;</description>
    <pubDate>Mon, 21 Sep 2026 23:21:39 GMT</pubDate>
    <dc:creator>pberna67</dc:creator>
    <dc:date>2026-09-21T23:21:39Z</dc:date>
    <item>
      <title>Remote access to FreeMASTER</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Remote-access-to-FreeMASTER/m-p/2415067#M2236</link>
      <description>&lt;P&gt;Dear All&lt;BR /&gt;&lt;BR /&gt;I would to access to FreeMaster running in a PC an connected to a target (LPC1766) via Jlink troughs a second PC connected in the same local network . Even if the connection to the local PC via e browser (Any),&amp;nbsp; using the simple example attached, works correctly, if move all files (attached) in a different PC, and finally I open the Test.htm in the remote browser, variable read don't work.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Respect the original NXP example where it indicated local-host, now the address is changed and it always point to the PC where FreeMASTER runs.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pberna67_0-1790032198582.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396633i7DC931A7515F8A0E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pberna67_0-1790032198582.png" alt="pberna67_0-1790032198582.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any idea of the reason of this problem ?&lt;BR /&gt;&lt;BR /&gt;Is it possible to create a Windows App Form in a remote PC that is able to connect (as a DCOM Client ??, don't know) to the FreeMASTER of the "local" PC where FreeMASTER (DCOM Server??) runs and it is connected to the target via Jlink emulator?,&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;1) What is the configuration of FreeMASTER of the local PC ?&lt;BR /&gt;2) How do I access via Visual Basic .NET&amp;nbsp; Form APP to the local PC from (where FreeMASTER runs) the Remote PC ?&lt;BR /&gt;&lt;BR /&gt;The reason of these questions is because my develop PC where Microsoft Visual Studio. .NET runs is not the same machine where FreeMASTER and the target board (LPC1766) are,&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2026 23:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Remote-access-to-FreeMASTER/m-p/2415067#M2236</guid>
      <dc:creator>pberna67</dc:creator>
      <dc:date>2026-09-21T23:21:39Z</dc:date>
    </item>
    <item>
      <title>Re: Remote access to FreeMASTER</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Remote-access-to-FreeMASTER/m-p/2415342#M2239</link>
      <description>&lt;P&gt;Problem solved &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt; sorry&lt;BR /&gt;It was related tothe fact that the 2 PCs have 2 different profiles , public and private, and so the FreeMASTER firewall setting blocks all port of public profile. If the profiles in both PC are set as private, the communication occours&lt;/P&gt;</description>
      <pubDate>Tue, 22 Sep 2026 12:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Remote-access-to-FreeMASTER/m-p/2415342#M2239</guid>
      <dc:creator>pberna67</dc:creator>
      <dc:date>2026-09-22T12:38:15Z</dc:date>
    </item>
  </channel>
</rss>