<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FreeMaster可以用来烧写hex/bin file吗 in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/FreeMaster%E5%8F%AF%E4%BB%A5%E7%94%A8%E6%9D%A5%E7%83%A7%E5%86%99hex-bin-file%E5%90%97/m-p/2249095#M2093</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the FreeMASTER can only communicate with the target MCU in runtime. It does not have any JTAG/flash-programming features.&lt;/P&gt;
&lt;P&gt;FreeMASTER can help to load the S-Record file and pass its content in small chunks to the MCU application for further processing (or even flashing), but the flashing itself needs to be implemented by the MCU application. See doc/flash_prog.pdf document included in the installation for more details about this feature.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
    <pubDate>Wed, 26 Nov 2025 07:55:26 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2025-11-26T07:55:26Z</dc:date>
    <item>
      <title>FreeMaster可以用来烧写hex/bin file吗</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMaster%E5%8F%AF%E4%BB%A5%E7%94%A8%E6%9D%A5%E7%83%A7%E5%86%99hex-bin-file%E5%90%97/m-p/2206651#M2086</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;想确认下FreeMaster可以烧写hex/bin文件吗，还是说它只是一个在线监控的工具？&lt;/P&gt;</description>
      <pubDate>Tue, 18 Nov 2025 08:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMaster%E5%8F%AF%E4%BB%A5%E7%94%A8%E6%9D%A5%E7%83%A7%E5%86%99hex-bin-file%E5%90%97/m-p/2206651#M2086</guid>
      <dc:creator>IdaWang</dc:creator>
      <dc:date>2025-11-18T08:59:26Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster可以用来烧写hex/bin file吗</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMaster%E5%8F%AF%E4%BB%A5%E7%94%A8%E6%9D%A5%E7%83%A7%E5%86%99hex-bin-file%E5%90%97/m-p/2249095#M2093</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the FreeMASTER can only communicate with the target MCU in runtime. It does not have any JTAG/flash-programming features.&lt;/P&gt;
&lt;P&gt;FreeMASTER can help to load the S-Record file and pass its content in small chunks to the MCU application for further processing (or even flashing), but the flashing itself needs to be implemented by the MCU application. See doc/flash_prog.pdf document included in the installation for more details about this feature.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 26 Nov 2025 07:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMaster%E5%8F%AF%E4%BB%A5%E7%94%A8%E6%9D%A5%E7%83%A7%E5%86%99hex-bin-file%E5%90%97/m-p/2249095#M2093</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2025-11-26T07:55:26Z</dc:date>
    </item>
  </channel>
</rss>