<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Freemaster Record function over CAN in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Record-function-over-CAN/m-p/2187418#M2073</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using S32K322 with PlatformSDK_S32K3_s32K322 version 4.0.0. The CAN speed is 500 kbit/s.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Osman&lt;/P&gt;</description>
    <pubDate>Thu, 16 Oct 2025 09:38:26 GMT</pubDate>
    <dc:creator>osmanorgut</dc:creator>
    <dc:date>2025-10-16T09:38:26Z</dc:date>
    <item>
      <title>Freemaster Record function over CAN</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Record-function-over-CAN/m-p/2187394#M2071</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am trying to use Freemaster tool to record a variable in my application.&lt;/P&gt;&lt;P&gt;I tried recording over serial and it is working as expected. When I switched to CAN, I can connect and use the scope functionality. However, recording function is somehow problematic. Small number of samples such as 10-20 recording is working as expected but when i set it to 100 (maximum samples to record is 230) it is not working and throwing below errors:&amp;nbsp;&lt;/P&gt;&lt;P&gt;- Recorder could not be initialised. Error: 0x858e0000 (Error in CAN/LIN response, bad toggle bit value.)&lt;/P&gt;&lt;P&gt;I am using freemaster driver&amp;nbsp;"3.0.7". Can you support me on this issue?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Osman&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 09:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Record-function-over-CAN/m-p/2187394#M2071</guid>
      <dc:creator>osmanorgut</dc:creator>
      <dc:date>2025-10-16T09:15:02Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster Record function over CAN</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Record-function-over-CAN/m-p/2187409#M2072</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;can you describe what is the target MCU and what MCUXpresso SDK version are you using?&amp;nbsp;There were some changes in CAN driver after version 3.0.7 (I guess this was MCUXpresso SDK v2.14).&lt;/P&gt;
&lt;P&gt;As the first step, I would recommend to try the latest version from MCUXpresso SDK (&lt;A href="https://mcuxpresso.nxp.com" target="_blank"&gt;https://mcuxpresso.nxp.com&lt;/A&gt;) for your board - ideally, just test the fmstr_can sample application and see if the Recorder runs fine. If not, I would suspect a hardware issue.&lt;/P&gt;
&lt;P&gt;If the fmstr_can example works well but your application does not, I would check the baudrate speed (what speed do you use?). Also make sure you use the&amp;nbsp;FLEXCAN_CalculateImprovedTimingValues in your initialization code to achieve the best possible timing setup.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 09:33:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Record-function-over-CAN/m-p/2187409#M2072</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2025-10-16T09:33:31Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster Record function over CAN</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Record-function-over-CAN/m-p/2187418#M2073</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using S32K322 with PlatformSDK_S32K3_s32K322 version 4.0.0. The CAN speed is 500 kbit/s.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Osman&lt;/P&gt;</description>
      <pubDate>Thu, 16 Oct 2025 09:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Record-function-over-CAN/m-p/2187418#M2073</guid>
      <dc:creator>osmanorgut</dc:creator>
      <dc:date>2025-10-16T09:38:26Z</dc:date>
    </item>
  </channel>
</rss>