<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 Support multi map file</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Support-multi-map-file/m-p/2075095#M1998</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;we use Freemaster with an S32K358, it's a multicore project.&lt;/P&gt;&lt;P&gt;Each core have a software and a map file.&lt;BR /&gt;&lt;BR /&gt;I don't find in Freemaster how to select 2 maps file to access variables of each core/ software .&lt;BR /&gt;&lt;BR /&gt;So how can I do that ? if not how can we use Freemaster on multicore with 2 software ?&lt;BR /&gt;&lt;BR /&gt;thank you&lt;BR /&gt;&lt;BR /&gt;Sophie&lt;/P&gt;</description>
    <pubDate>Mon, 07 Apr 2025 10:55:48 GMT</pubDate>
    <dc:creator>sobo</dc:creator>
    <dc:date>2025-04-07T10:55:48Z</dc:date>
    <item>
      <title>Support multi map file</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Support-multi-map-file/m-p/2075095#M1998</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;we use Freemaster with an S32K358, it's a multicore project.&lt;/P&gt;&lt;P&gt;Each core have a software and a map file.&lt;BR /&gt;&lt;BR /&gt;I don't find in Freemaster how to select 2 maps file to access variables of each core/ software .&lt;BR /&gt;&lt;BR /&gt;So how can I do that ? if not how can we use Freemaster on multicore with 2 software ?&lt;BR /&gt;&lt;BR /&gt;thank you&lt;BR /&gt;&lt;BR /&gt;Sophie&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 10:55:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Support-multi-map-file/m-p/2075095#M1998</guid>
      <dc:creator>sobo</dc:creator>
      <dc:date>2025-04-07T10:55:48Z</dc:date>
    </item>
    <item>
      <title>Re: Support multi map file</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Support-multi-map-file/m-p/2075156#M1999</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;FreeMASTER can only communicate to one target. This is similar to multi-processor setup, you can run multiple instances of FreeMASTERs and each can may communicate with one target core. Each core shall use a different serial port or different CAN frame identifiers.&lt;/P&gt;
&lt;P&gt;In case you use a JTAG direct memory access, you could theoretically observe both operational memory areas used by the two cores using a single FreeMASTER session - in this case you need a mechanism how to join the two map files into one and parse it with a Regular expression parser. Unfortunately, FreeMASTER has no built-in support to simplify this task.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 12:12:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Support-multi-map-file/m-p/2075156#M1999</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2025-04-07T12:12:43Z</dc:date>
    </item>
  </channel>
</rss>