<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: Freemaster could not open communication error</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064471#M1961</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;do you mean that the same port on the same cable works well with another FreeMASTER project? Then it must be something wrong with the communication settings in this particular project.&lt;/P&gt;
&lt;P&gt;Try to avoid port probing in the project Options. Just select a real COM port Instead of COM_ALL.&lt;/P&gt;
&lt;P&gt;If this does not help, please upload a FreeMASTER project which works well. I shall be able to see what is different.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;</description>
    <pubDate>Wed, 19 Mar 2025 08:00:50 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2025-03-19T08:00:50Z</dc:date>
    <item>
      <title>Freemaster could not open communication error</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2063952#M1960</link>
      <description>&lt;P&gt;Hi NXP Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm working with the project attached on MBDT using&amp;nbsp;S32K3X8EVB-Q289.&lt;/P&gt;&lt;P&gt;I've encoutered a problem with freemaster that i don' know how to solve:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="popup_fm.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/328639i02BC9C1228E42710/image-size/medium?v=v2&amp;amp;px=400" role="button" title="popup_fm.png" alt="popup_fm.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;popup_fm.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm quite sure that the port is available ... I've tried an other project without changing the cable connection and it works...&lt;/P&gt;&lt;P&gt;So i don't know where to look to find a solution...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Tue, 18 Mar 2025 16:30:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2063952#M1960</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2025-03-18T16:30:30Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster could not open communication error</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064471#M1961</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;do you mean that the same port on the same cable works well with another FreeMASTER project? Then it must be something wrong with the communication settings in this particular project.&lt;/P&gt;
&lt;P&gt;Try to avoid port probing in the project Options. Just select a real COM port Instead of COM_ALL.&lt;/P&gt;
&lt;P&gt;If this does not help, please upload a FreeMASTER project which works well. I shall be able to see what is different.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 08:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064471#M1961</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2025-03-19T08:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster could not open communication error</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064475#M1962</link>
      <description>Hi Michal,&lt;BR /&gt;Yes i maen that... I've also tried to change the port selection, selecting the real COM port but nothing changed...&lt;BR /&gt;If you see in the xip folder there is the freemaster project that i use to test&lt;BR /&gt;&lt;BR /&gt;BR,&lt;BR /&gt;Simon</description>
      <pubDate>Wed, 19 Mar 2025 08:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064475#M1962</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2025-03-19T08:04:27Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster could not open communication error</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064505#M1963</link>
      <description>&lt;P&gt;Hi Michal,&lt;/P&gt;&lt;P&gt;I've find out, comparing the mexes files of the two project, that AIPS_PLAT_CLK was different...&lt;/P&gt;&lt;P&gt;In the bad project it's 80MHz, in the good one 120MHz...&lt;/P&gt;&lt;P&gt;Changing the value from 80 to 120 in the bad project and changing the FLEXCAN0CLK divider, in order to have 40MHz, make it works!&lt;/P&gt;&lt;P&gt;So my question is: Why the AIPS_PLAT_CLK interfeer with the freemaster comunication as freemaster is configured to work with LPUART13 (USB UART(serial) Interface on EVL BOARD) which have a AIPS_SLOW_CLK source? Is there something else that i'm missing?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I attached the Mex file of the good project, you ha compare with the one inside my zip to notice the differeces.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 08:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064505#M1963</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2025-03-19T08:33:34Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster could not open communication error</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064590#M1965</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I need to defer this issue to my colleagues in charge of S32K platform. I can only help with general FreeMASTER topic.&lt;/P&gt;
&lt;P&gt;I'm not sure how the PLAT clock affects UART baudrate, but there is one trick that may help to confirm that this is the real issue.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In freemaster_cfg.h, you can define the &lt;STRONG&gt;FMSTR_DEBUG_TX&lt;/STRONG&gt; to 1 and attach to a board with a plain terminal application (e.g. TeraTerm). You should see a sequence&amp;nbsp;&lt;STRONG&gt;+©V&amp;nbsp;&lt;/STRONG&gt;printed periodically. by the board.&amp;nbsp; If not, there is indeed a clock issue and you can attach a logic analyzer to SCI TX pin to see a real baudrate used.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 09:36:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-could-not-open-communication-error/m-p/2064590#M1965</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2025-03-19T09:36:51Z</dc:date>
    </item>
  </channel>
</rss>