<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: s32k312 freemaster</title>
    <link>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1986154#M1927</link>
    <description>&lt;P&gt;In FreeMASTER, I set the mask of MB1 to 0x7FF, allowing only FreeMASTER's command CAN IDs to enter this mailbox, while all other CAN IDs are directed to other mailboxes. After that, sending and receiving will follow the polling mode logic.&lt;/P&gt;</description>
    <pubDate>Fri, 01 Nov 2024 08:59:49 GMT</pubDate>
    <dc:creator>fengba_360</dc:creator>
    <dc:date>2024-11-01T08:59:49Z</dc:date>
    <item>
      <title>s32k312 freemaster</title>
      <link>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1982541#M1909</link>
      <description>&lt;P&gt;I am using CAN communication for monitoring with S32K312 FreeMaster, and I have a question to consult. Does FreeMaster support using the same CAN channel as the application? For example, on this CAN channel, can I both send and receive CAN IDs for FreeMaster, and simultaneously send other application-specific CAN IDs?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Oct 2024 01:44:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1982541#M1909</guid>
      <dc:creator>fengba_360</dc:creator>
      <dc:date>2024-10-28T01:44:58Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 freemaster</title>
      <link>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1984719#M1911</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238047"&gt;@fengba_360&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;The same CAN instance cannot be used simultaneously, both by FreeMASTER and by application custom logic.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Oct 2024 12:02:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1984719#M1911</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2024-10-30T12:02:02Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 freemaster</title>
      <link>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1985361#M1919</link>
      <description>I seem to have solved this problem through can polling.After initial testing, FreeMaster can now work simultaneously with the application CAN.</description>
      <pubDate>Thu, 31 Oct 2024 07:40:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1985361#M1919</guid>
      <dc:creator>fengba_360</dc:creator>
      <dc:date>2024-10-31T07:40:04Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 freemaster</title>
      <link>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1985375#M1920</link>
      <description>&lt;P&gt;Good to hear that it worked for you.&lt;/P&gt;
&lt;P&gt;Were there any extra configuration you had to make (in FreeMASTER or SDK) or it was enough to switch to CAN polling mode ?&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 08:17:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1985375#M1920</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2024-10-31T08:17:52Z</dc:date>
    </item>
    <item>
      <title>Re: s32k312 freemaster</title>
      <link>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1986154#M1927</link>
      <description>&lt;P&gt;In FreeMASTER, I set the mask of MB1 to 0x7FF, allowing only FreeMASTER's command CAN IDs to enter this mailbox, while all other CAN IDs are directed to other mailboxes. After that, sending and receiving will follow the polling mode logic.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Nov 2024 08:59:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/s32k312-freemaster/m-p/1986154#M1927</guid>
      <dc:creator>fengba_360</dc:creator>
      <dc:date>2024-11-01T08:59:49Z</dc:date>
    </item>
  </channel>
</rss>