<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Use FreeMASTER with i.MX8M-Plus in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Use-FreeMASTER-with-i-MX8M-Plus/m-p/1980052#M1904</link>
    <description>&lt;P&gt;The platform support for FreeMASTER&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER" target="_self"&gt;https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER&lt;/A&gt;&lt;/P&gt;&lt;P&gt;doesn't mention the Cortex-M of i.MX8M-Plus.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can FreeMASTER be used with it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 23 Oct 2024 09:16:46 GMT</pubDate>
    <dc:creator>vix</dc:creator>
    <dc:date>2024-10-23T09:16:46Z</dc:date>
    <item>
      <title>Use FreeMASTER with i.MX8M-Plus</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Use-FreeMASTER-with-i-MX8M-Plus/m-p/1980052#M1904</link>
      <description>&lt;P&gt;The platform support for FreeMASTER&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER" target="_self"&gt;https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER&lt;/A&gt;&lt;/P&gt;&lt;P&gt;doesn't mention the Cortex-M of i.MX8M-Plus.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can FreeMASTER be used with it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Oct 2024 09:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Use-FreeMASTER-with-i-MX8M-Plus/m-p/1980052#M1904</guid>
      <dc:creator>vix</dc:creator>
      <dc:date>2024-10-23T09:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: Use FreeMASTER with i.MX8M-Plus</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Use-FreeMASTER-with-i-MX8M-Plus/m-p/1984743#M1914</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;unfortunately, we do not have any out-of-box example demonstrating the FreeMASTER use on i.MX8/9.&lt;/P&gt;
&lt;P&gt;However, running the code adopted from any Cortex-M device such as MCXN947, i.MX-RT1060 or any Kinetis/LPC device shall be quite smooth. The only what needs to be done is to configure pins and UART clocks.&lt;/P&gt;
&lt;P&gt;In case you use the MCUXpresso SDK for the CortexM development, it shall be even simpler as the initialization code will be very similar.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 30 Oct 2024 12:33:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Use-FreeMASTER-with-i-MX8M-Plus/m-p/1984743#M1914</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2024-10-30T12:33:43Z</dc:date>
    </item>
    <item>
      <title>Re: Use FreeMASTER with i.MX8M-Plus</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Use-FreeMASTER-with-i-MX8M-Plus/m-p/1985392#M1921</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34487"&gt;@MichalH&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a lot of applications running on M7 core of iMX8M-Plus.&lt;/P&gt;&lt;P&gt;Based on what I saw, printing on the UART is too slow to be non-intrusive (the baud rate of UAERT is too slow). At the moment, UART printing is the only way for me to debug, but with a lot of limitations.&lt;/P&gt;&lt;P&gt;FreeMASTER seems promising because I see in the picture that it supports JTAG/SWD.&lt;/P&gt;&lt;P&gt;But I learnt that using JTAG/SWD on M7 of iMX8MP is a little bit tricky.&lt;/P&gt;&lt;P&gt;Do you know if this works?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Oct 2024 08:31:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Use-FreeMASTER-with-i-MX8M-Plus/m-p/1985392#M1921</guid>
      <dc:creator>vix</dc:creator>
      <dc:date>2024-10-31T08:31:02Z</dc:date>
    </item>
  </channel>
</rss>