<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Freemaster on CAN for s12z in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-on-CAN-for-s12z/m-p/1970100#M1895</link>
    <description>&lt;P&gt;If I understand well: Freemaster 3.2 is not compatible with Freemaster driver V2.0, at least for the CAN (BDM and UART works well).&lt;/P&gt;&lt;P&gt;Where do I find FreeMASTER Communication Driver 3.0 (S12)?&lt;/P&gt;</description>
    <pubDate>Wed, 09 Oct 2024 16:07:25 GMT</pubDate>
    <dc:creator>tsh18609</dc:creator>
    <dc:date>2024-10-09T16:07:25Z</dc:date>
    <item>
      <title>Freemaster on CAN for s12z</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-on-CAN-for-s12z/m-p/1969904#M1893</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to enable Freemaster over CAN (instead of UART or BDM) on my project using the mc9s12zvmc128 device. Is this supported?&lt;/P&gt;&lt;P&gt;My materials:&lt;/P&gt;&lt;P&gt;- FreeMASTER_Serial_Communication_Driver_V2.0&lt;/P&gt;&lt;P&gt;- Freemaster 3.2&lt;/P&gt;&lt;P&gt;- IXXAT USB-to-CAN Compact device&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 11:37:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-on-CAN-for-s12z/m-p/1969904#M1893</guid>
      <dc:creator>tsh18609</dc:creator>
      <dc:date>2024-10-09T11:37:24Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster on CAN for s12z</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-on-CAN-for-s12z/m-p/1970100#M1895</link>
      <description>&lt;P&gt;If I understand well: Freemaster 3.2 is not compatible with Freemaster driver V2.0, at least for the CAN (BDM and UART works well).&lt;/P&gt;&lt;P&gt;Where do I find FreeMASTER Communication Driver 3.0 (S12)?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 16:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-on-CAN-for-s12z/m-p/1970100#M1895</guid>
      <dc:creator>tsh18609</dc:creator>
      <dc:date>2024-10-09T16:07:25Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster on CAN for s12z</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-on-CAN-for-s12z/m-p/1970995#M1896</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;FreeMASTER 3.x supports all versions of communication protocol, so it is also compatible with Serial Driver 2.0 on the S12Z. FreeMASTER detects the protocol version automatically.&lt;/P&gt;
&lt;P&gt;I don't think the new driver has been ported back to S12Z, but the example in the 2.0 driver package should work just fine.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 06:12:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-on-CAN-for-s12z/m-p/1970995#M1896</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2024-10-10T06:12:33Z</dc:date>
    </item>
  </channel>
</rss>