<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 Re: FreeMaster For FlexRay</title>
    <link>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044447#M184</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, FreeMASTER&amp;nbsp;cannot monitor raw signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Short clarification: FreeMASTER has a functionality called "oscilloscope" (to not be confused with signal processing device). It provides the capability to plot&amp;nbsp;one or multiple embedded application variables on a chart widget similar to how signal data is visualized on an actual oscilloscope display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Iulian&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Jul 2020 13:09:36 GMT</pubDate>
    <dc:creator>iulian_stan</dc:creator>
    <dc:date>2020-07-01T13:09:36Z</dc:date>
    <item>
      <title>FreeMaster For FlexRay</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044444#M181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can I use FreeMaster to monitor FlexRay Transmitted frames from a node ?&lt;/P&gt;&lt;P&gt;If yes which document i can refer to use FreeMaster.&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;A href="https://www.nxp.com/design/development-boards/automotive-development-platforms/mpc57xx-mcu-platforms/mpc5748g-development-board-for-secure-gateway:DEVKIT-MPC5748G"&gt;DEVKIT-MPC5748G&lt;/A&gt;&amp;nbsp;development board&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jun 2020 07:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044444#M181</guid>
      <dc:creator>Deepak1</dc:creator>
      <dc:date>2020-06-30T07:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster For FlexRay</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044445#M182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Deepak"&gt;Deepak&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FreeMASTER&amp;nbsp;won't help much&amp;nbsp;with such tasks as communication bus analysis/sniffing. It's main purpose is to monitor and control your embedded application variables. You could still be able to&amp;nbsp;get some&amp;nbsp;data going through&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;FlexRay&lt;SPAN&gt;&amp;nbsp;by copying the frames into a variable and display it in FreeMASTER UI, but that&amp;nbsp;does not guarantee you&amp;nbsp;the same accuracy as a dedicated analyser, because FreeMASTER&amp;nbsp;may not read data from the target at the same rate, at which dataframes come from FlexRay.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;An example of a task that would be a better fit for FreeMASTER is to&amp;nbsp;monitor communication statistics (ex: number of frames send/received), but it would still require&amp;nbsp;a piece a piece of logic, that gathers those statistics and stores them, implemented in the embedded application.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Iulian&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2020 08:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044445#M182</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-07-01T08:34:00Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster For FlexRay</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044446#M183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Iulian,&lt;/P&gt;&lt;P&gt;Can I use FreeMaster as like o&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;scilloscope to monitor the flexray tx and rx frames signals. If yes then, it is possible to decode the signals.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2020 12:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044446#M183</guid>
      <dc:creator>Deepak1</dc:creator>
      <dc:date>2020-07-01T12:43:03Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMaster For FlexRay</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044447#M184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No, FreeMASTER&amp;nbsp;cannot monitor raw signals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Short clarification: FreeMASTER has a functionality called "oscilloscope" (to not be confused with signal processing device). It provides the capability to plot&amp;nbsp;one or multiple embedded application variables on a chart widget similar to how signal data is visualized on an actual oscilloscope display.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Iulian&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jul 2020 13:09:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMaster-For-FlexRay/m-p/1044447#M184</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2020-07-01T13:09:36Z</dc:date>
    </item>
  </channel>
</rss>