<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Calibration features in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Calibration-features/m-p/1937262#M1794</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wonder if FreeMaster is capable of being used as a calibration tool. For example, calibrate a thermistor with a NXP board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another question on top of this: i&lt;SPAN&gt;s it possible to apply a function to a raw signal before it is displayed on a graph in FreeMaster?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 21 Aug 2024 08:56:41 GMT</pubDate>
    <dc:creator>Vast-Horizon</dc:creator>
    <dc:date>2024-08-21T08:56:41Z</dc:date>
    <item>
      <title>Calibration features</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Calibration-features/m-p/1937262#M1794</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I wonder if FreeMaster is capable of being used as a calibration tool. For example, calibrate a thermistor with a NXP board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another question on top of this: i&lt;SPAN&gt;s it possible to apply a function to a raw signal before it is displayed on a graph in FreeMaster?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Aug 2024 08:56:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Calibration-features/m-p/1937262#M1794</guid>
      <dc:creator>Vast-Horizon</dc:creator>
      <dc:date>2024-08-21T08:56:41Z</dc:date>
    </item>
    <item>
      <title>Re: Calibration features</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Calibration-features/m-p/1937299#M1795</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/232747"&gt;@Vast-Horizon&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Yes, you can use FreeMASTER as calibration tool. Here's an example of how it could be used in such scenario:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;Implement the algorithm in the embedded application&lt;/LI&gt;
&lt;LI&gt;Store algorithm parameters in global volatile variables&lt;/LI&gt;
&lt;LI&gt;Use FreeMASTER to read algorithm parameters at runtime&lt;/LI&gt;
&lt;LI&gt;Use FreeMASTER to update parameter values to fine tune the algorithm&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;You can also apply transformation functions on the variables before those are displayed. This option is available in the Variable menu (Project -&amp;gt; Variables -&amp;gt; Edit):&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Untitled.png" style="width: 595px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/294509i53E8C611659B1574/image-size/large?v=v2&amp;amp;px=999" role="button" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Note: transformations are applicable only to REAL values (top right option)&lt;/P&gt;
&lt;P&gt;Hope it helps,&lt;BR /&gt;Iulian&lt;/P&gt;</description>
      <pubDate>Wed, 21 Aug 2024 09:17:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Calibration-features/m-p/1937299#M1795</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2024-08-21T09:17:41Z</dc:date>
    </item>
  </channel>
</rss>