<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCAT motor parameter identification (see AN4986) missing in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/MCAT-motor-parameter-identification-see-AN4986-missing/m-p/1823598#M1657</link>
    <description>&lt;P&gt;In AppNote AN4986 there is the detailed description of the motor parameter identification and the picture shows a special tab "Motor Identif".&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MotorIdentif_AN4986.jpg" style="width: 455px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/267107i8E7402EF7ED85E14/image-dimensions/455x423?v=v2" width="455" height="423" role="button" title="MotorIdentif_AN4986.jpg" alt="MotorIdentif_AN4986.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MotorIdentif_AN4986.jpg&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;Even custom power boards are supported!&lt;BR /&gt;&lt;BR /&gt;I want to use the S32K144 Evalboard with the DevKit MOTORGD and want to identify parameters of some unknown, small motors.&lt;BR /&gt;Where can this MCAT-functionality be found and which firmware is necessary to support this? Is it still available?&lt;/P&gt;</description>
    <pubDate>Thu, 07 Mar 2024 19:17:39 GMT</pubDate>
    <dc:creator>HolgerMC</dc:creator>
    <dc:date>2024-03-07T19:17:39Z</dc:date>
    <item>
      <title>MCAT motor parameter identification (see AN4986) missing</title>
      <link>https://community.nxp.com/t5/FreeMASTER/MCAT-motor-parameter-identification-see-AN4986-missing/m-p/1823598#M1657</link>
      <description>&lt;P&gt;In AppNote AN4986 there is the detailed description of the motor parameter identification and the picture shows a special tab "Motor Identif".&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MotorIdentif_AN4986.jpg" style="width: 455px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/267107i8E7402EF7ED85E14/image-dimensions/455x423?v=v2" width="455" height="423" role="button" title="MotorIdentif_AN4986.jpg" alt="MotorIdentif_AN4986.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MotorIdentif_AN4986.jpg&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;Even custom power boards are supported!&lt;BR /&gt;&lt;BR /&gt;I want to use the S32K144 Evalboard with the DevKit MOTORGD and want to identify parameters of some unknown, small motors.&lt;BR /&gt;Where can this MCAT-functionality be found and which firmware is necessary to support this? Is it still available?&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 19:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/MCAT-motor-parameter-identification-see-AN4986-missing/m-p/1823598#M1657</guid>
      <dc:creator>HolgerMC</dc:creator>
      <dc:date>2024-03-07T19:17:39Z</dc:date>
    </item>
  </channel>
</rss>