<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 Re: Freemaster Query</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Query/m-p/1774678#M1564</link>
    <description>&lt;P&gt;Yes, BLDC app is loaded in the target MCU Board.&lt;BR /&gt;PC through code worrier BLDC application code is loaded on MCU board through P&amp;amp;E debugger and then connect MCU board USB/SCI free master to PC through USB and opening project in Free master and starting Communication. There is communication error is show.&lt;/P&gt;</description>
    <pubDate>Thu, 14 Dec 2023 09:43:05 GMT</pubDate>
    <dc:creator>21</dc:creator>
    <dc:date>2023-12-14T09:43:05Z</dc:date>
    <item>
      <title>Freemaster Query</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Query/m-p/1770437#M1554</link>
      <description>&lt;P&gt;When I open MC9S12ZVML128_BLDC_Hall.pmp with FreeMASTER3.0, the following prompt appears. How do I solve this problem?&lt;BR /&gt;Error show-&lt;BR /&gt;1.symbol not found.&lt;BR /&gt;2.communication Error.&lt;BR /&gt;3.If started the communication then, not getting the values if variable&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 06:10:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Query/m-p/1770437#M1554</guid>
      <dc:creator>21</dc:creator>
      <dc:date>2023-12-07T06:10:02Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster Query</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Query/m-p/1770684#M1557</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;do you have the BLDC application loaded in the target MCU board and is the board properly connected to the PC?&lt;/P&gt;
&lt;P&gt;Please describe your hardware setup, what application you run in the MCU and how is your PC connected to the board.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Thu, 07 Dec 2023 10:56:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Query/m-p/1770684#M1557</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-12-07T10:56:16Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster Query</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Query/m-p/1774678#M1564</link>
      <description>&lt;P&gt;Yes, BLDC app is loaded in the target MCU Board.&lt;BR /&gt;PC through code worrier BLDC application code is loaded on MCU board through P&amp;amp;E debugger and then connect MCU board USB/SCI free master to PC through USB and opening project in Free master and starting Communication. There is communication error is show.&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 09:43:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Query/m-p/1774678#M1564</guid>
      <dc:creator>21</dc:creator>
      <dc:date>2023-12-14T09:43:05Z</dc:date>
    </item>
  </channel>
</rss>