<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1714027#M1428</link>
    <description>&lt;P&gt;Hello Luca,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;yes as discussed in other two posts in this forum, the FreeMASTER Edge browser component crashes after a recent Windows/Edge update deployed by Microsoft. This issue affects all FreeMASTER 3.2.x versions with Edge support.&lt;/P&gt;
&lt;P&gt;As Edge is the default component used to render the Welcome page, the FreeMASTER crashes as soon as you run it. When you run FreeMASTER by opening a project which uses IE or CEF engine to render HTML, then the FreeMASTER works normally (until you do File/New).&lt;/P&gt;
&lt;P&gt;Another workaround is to rename the&amp;nbsp;"c:\NXP\FreeMASTER 3.2\FreeMASTER\html"&amp;nbsp; to html.bak to prevent the Welcome page to load. But still using Edge engine to render project-specific content may have issues.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;We have identified the root cause of the issue and we are now working on hotfix release. This should be out during the next week - early Sep/2023.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Thanks for staying with us,&lt;BR /&gt;Michal&lt;/P&gt;</description>
    <pubDate>Wed, 30 Aug 2023 12:34:55 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2023-08-30T12:34:55Z</dc:date>
    <item>
      <title>Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1713998#M1426</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Today my Freemaster 3.2 doesn't want to work.. It crashes silently every time I launch it (also tried to launch from command line, in case there would be some error message there but nothing).&lt;/P&gt;&lt;P&gt;I have tried to uninstall and reinstall latest version from the website, problem persists.&lt;/P&gt;&lt;P&gt;I have used it a million times until two days ago. What could be wrong in my laptop that I should check?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 11:19:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1713998#M1426</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2023-08-30T11:19:11Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1714000#M1427</link>
      <description>&lt;P&gt;If I double click in Windows on a freemaster project, the application starts correctly actually. Then it crashes again if from the application I create a new project.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 11:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1714000#M1427</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2023-08-30T11:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1714027#M1428</link>
      <description>&lt;P&gt;Hello Luca,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;yes as discussed in other two posts in this forum, the FreeMASTER Edge browser component crashes after a recent Windows/Edge update deployed by Microsoft. This issue affects all FreeMASTER 3.2.x versions with Edge support.&lt;/P&gt;
&lt;P&gt;As Edge is the default component used to render the Welcome page, the FreeMASTER crashes as soon as you run it. When you run FreeMASTER by opening a project which uses IE or CEF engine to render HTML, then the FreeMASTER works normally (until you do File/New).&lt;/P&gt;
&lt;P&gt;Another workaround is to rename the&amp;nbsp;"c:\NXP\FreeMASTER 3.2\FreeMASTER\html"&amp;nbsp; to html.bak to prevent the Welcome page to load. But still using Edge engine to render project-specific content may have issues.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;We have identified the root cause of the issue and we are now working on hotfix release. This should be out during the next week - early Sep/2023.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Thanks for staying with us,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 12:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1714027#M1428</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-08-30T12:34:55Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1714033#M1429</link>
      <description>&lt;P&gt;Thank you &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34487"&gt;@MichalH&lt;/a&gt; and sorry for asking duplicate questions. I did check for similar topics but maybe too briefly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;</description>
      <pubDate>Wed, 30 Aug 2023 12:39:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1714033#M1429</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2023-08-30T12:39:11Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1717834#M1432</link>
      <description>&lt;P&gt;Hello Luca,&lt;/P&gt;
&lt;P&gt;the issue should now be fixed.&amp;nbsp;Please update to 3.2.2.2 available at &lt;A href="http://www.nxp.com/freemaster" target="_blank"&gt;www.nxp.com/freemaster&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Please close this thread if you test the hotfix successfully.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Sep 2023 07:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1717834#M1432</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-09-06T07:54:33Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1718747#M1435</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34487"&gt;@MichalH&lt;/a&gt;&lt;/P&gt;&lt;P&gt;Problem solved. Thanks!&lt;/P&gt;</description>
      <pubDate>Thu, 07 Sep 2023 10:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1718747#M1435</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2023-09-07T10:43:22Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1723054#M1450</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are experiencing the same issue&lt;/P&gt;&lt;P&gt;Freemaster last downloadable version on Win10 with last updates&lt;/P&gt;&lt;P&gt;HTML directory rename workaround does not work&lt;/P&gt;&lt;P&gt;Trying to open freemaster through a projet does not work either.&lt;/P&gt;&lt;P&gt;Are there other any fixes to test?&lt;/P&gt;</description>
      <pubDate>Thu, 14 Sep 2023 10:25:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1723054#M1450</guid>
      <dc:creator>diniz</dc:creator>
      <dc:date>2023-09-14T10:25:40Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1723060#M1451</link>
      <description>Are you sure that you are using the latest 3.2.2.2 version from the website? That should solve the problem. It did for me on Windows 10 of course.</description>
      <pubDate>Thu, 14 Sep 2023 10:33:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1723060#M1451</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2023-09-14T10:33:23Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1723155#M1456</link>
      <description>&lt;P&gt;Yes i'm sure.&lt;/P&gt;&lt;P&gt;You can see on the picture attached.&lt;/P&gt;&lt;P&gt;A problem with a "libcef.dll"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 14 Sep 2023 12:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1723155#M1456</guid>
      <dc:creator>diniz</dc:creator>
      <dc:date>2023-09-14T12:51:40Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 Deskop Application Crashes when launched</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1723162#M1457</link>
      <description>&lt;P&gt;Dear Denis,&lt;/P&gt;
&lt;P&gt;this seems to be a different issue than the Edge browser issue we were fixing in 3.2.2.2. Maybe partly related as the Edge internally uses Chromium engine, but we need to investigate.&lt;/P&gt;
&lt;P&gt;Please open a new thread on this community and describe again. Also state if the issue can be replicated on multiple computers and/or if any computer exists which is not affected.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you!&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Thu, 14 Sep 2023 13:00:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Deskop-Application-Crashes-when-launched/m-p/1723162#M1457</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-09-14T13:00:39Z</dc:date>
    </item>
  </channel>
</rss>