<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: No Freemaster CMSIS-DAP connection to LPC5536-EVK in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/No-Freemaster-CMSIS-DAP-connection-to-LPC5536-EVK/m-p/1686317#M1388</link>
    <description>&lt;P&gt;OK thanks.&lt;/P&gt;&lt;P&gt;Already tested, now it's fine.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jul 2023 07:05:41 GMT</pubDate>
    <dc:creator>AlbertoGarlassi</dc:creator>
    <dc:date>2023-07-12T07:05:41Z</dc:date>
    <item>
      <title>No Freemaster CMSIS-DAP connection to LPC5536-EVK</title>
      <link>https://community.nxp.com/t5/FreeMASTER/No-Freemaster-CMSIS-DAP-connection-to-LPC5536-EVK/m-p/1685897#M1386</link>
      <description>&lt;P&gt;Hello, I'm able to load and debug this board with MCUXpresso, the debugger is shown&amp;nbsp; as MCU-LINK on board (r0C7) CMSIS-DAP V3.108.&lt;/P&gt;&lt;P&gt;But Freemaster, set as "CMSIS-MASTER CMSIS-DAP Communication Plugin" and pressing "Configure" shows that no device is present.&lt;/P&gt;&lt;P&gt;Configuring with the communication wizard brings the same result.&lt;/P&gt;&lt;P&gt;This happens with a closed MCUXpresso, so the interface is not already in use.&lt;/P&gt;&lt;P&gt;Reinstalled as administrator: no success.&lt;/P&gt;&lt;P&gt;Am I missing something?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 15:44:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/No-Freemaster-CMSIS-DAP-connection-to-LPC5536-EVK/m-p/1685897#M1386</guid>
      <dc:creator>AlbertoGarlassi</dc:creator>
      <dc:date>2023-07-11T15:44:05Z</dc:date>
    </item>
    <item>
      <title>Re: No Freemaster CMSIS-DAP connection to LPC5536-EVK</title>
      <link>https://community.nxp.com/t5/FreeMASTER/No-Freemaster-CMSIS-DAP-connection-to-LPC5536-EVK/m-p/1686291#M1387</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;the MCU-LINK v3.108 brings a new version of CMSIS-DAP interface (v2.1) which is not compatible with FreeMASTER 3.2.1 and earlier versions. The FreeMASTER 3.2.2 is going to support this CMSIS-DAP version soon and will also remain backward compatible with older versions.&lt;/P&gt;
&lt;P&gt;As a temporary workaround before FreeMASTER 3.2.2 is available, you can downgrade your MCU-LINK to versions prior to 3.108.&lt;/P&gt;
&lt;P&gt;We are sorry for the inconvenience.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 06:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/No-Freemaster-CMSIS-DAP-connection-to-LPC5536-EVK/m-p/1686291#M1387</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-07-12T06:35:38Z</dc:date>
    </item>
    <item>
      <title>Re: No Freemaster CMSIS-DAP connection to LPC5536-EVK</title>
      <link>https://community.nxp.com/t5/FreeMASTER/No-Freemaster-CMSIS-DAP-connection-to-LPC5536-EVK/m-p/1686317#M1388</link>
      <description>&lt;P&gt;OK thanks.&lt;/P&gt;&lt;P&gt;Already tested, now it's fine.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jul 2023 07:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/No-Freemaster-CMSIS-DAP-connection-to-LPC5536-EVK/m-p/1686317#M1388</guid>
      <dc:creator>AlbertoGarlassi</dc:creator>
      <dc:date>2023-07-12T07:05:41Z</dc:date>
    </item>
  </channel>
</rss>