<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669290#M1364</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for getting back to me.&lt;BR /&gt;I'm using MCU-Link pro (SWD) as the connection to the board. The TSA is disabled.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="siamak_riahi_im_0-1686744321814.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227680i5CD1A144474D748A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="siamak_riahi_im_0-1686744321814.png" alt="siamak_riahi_im_0-1686744321814.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;siamak_riahi_im_0-1686744321814.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Jun 2023 12:05:41 GMT</pubDate>
    <dc:creator>Sam_im</dc:creator>
    <dc:date>2023-06-14T12:05:41Z</dc:date>
    <item>
      <title>Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1668515#M1362</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I 'm working on a master-slave multicore project using a&amp;nbsp;&lt;SPAN&gt;i.MX RT1170 EVK compatible board (MaaxBoardRT). Freemaster is working greate on the variables from master project (CM7) but I have problem loading variables on slave project (CM4).&amp;nbsp;&lt;BR /&gt;I tried to add map files from CM4 debug folder and add slave variables from there but not value is showing.&lt;BR /&gt;Is there any way to access those slave project variables also in FreeMaster?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance,&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Jun 2023 15:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1668515#M1362</guid>
      <dc:creator>Sam_im</dc:creator>
      <dc:date>2023-06-13T15:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669005#M1363</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;can you tell more about your connection from the PC to the target and if you use the TSA feature?&lt;/P&gt;
&lt;P&gt;If using serial line, CAN, or USB, the freemaster accesses the core which implements the communication (CM7 in this case I guess). So the CM4&amp;nbsp; variable visibility and addresses depend on how the CM7 sees them in its address space. Normally, the CM7 should be able to see the OCRAM space of CM4 (0x20200000).&lt;/P&gt;
&lt;P&gt;Be aware that if you use the TSA feature and TSA_SAFETY feature (enabled in freemaster_cfg.h), the access to "unknown" variables can be actively blocked by freemaster driver unless you put them all to any TSA table. You can experimentally disable the TSA and only use addresses loaded from the ELF file.&lt;/P&gt;
&lt;P&gt;In case of using JTAG direct memory access (CMSIS-DAP etc.), all memories should be accessible, unless the JTAG is disabled.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 07:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669005#M1363</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-06-14T07:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669290#M1364</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;Thanks for getting back to me.&lt;BR /&gt;I'm using MCU-Link pro (SWD) as the connection to the board. The TSA is disabled.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="siamak_riahi_im_0-1686744321814.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/227680i5CD1A144474D748A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="siamak_riahi_im_0-1686744321814.png" alt="siamak_riahi_im_0-1686744321814.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;siamak_riahi_im_0-1686744321814.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 12:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669290#M1364</guid>
      <dc:creator>Sam_im</dc:creator>
      <dc:date>2023-06-14T12:05:41Z</dc:date>
    </item>
    <item>
      <title>Re: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669296#M1365</link>
      <description>&lt;P&gt;OK.&amp;nbsp;When using SWD, the TSA does not matter. The FreeMASTER accesses the memory directly over DAP MEM-AP. Can you describe what addresses are not accessible? What memory is used as RAM by your CM4 project?&lt;/P&gt;
&lt;P&gt;What values does the FreeMASTER show for the variables which do not work? Does it show zeros or question-marks?&lt;/P&gt;
&lt;P&gt;In my case, the CM4 OCRAM (0x20200000) can be accessed in FreeMASTER over CMSIS-DAP well - I have created a FreeMASTER variable at this address and it can be both read and written.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 12:13:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669296#M1365</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-06-14T12:13:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669317#M1366</link>
      <description>&lt;P&gt;I try to import cm4 axf map file from the slave project debug folder. you can consider for example&amp;nbsp;avValue variable from the list which has the address of&amp;nbsp;0x1ffe86c8;&lt;BR /&gt;I've attached the list.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 12:43:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669317#M1366</guid>
      <dc:creator>Sam_im</dc:creator>
      <dc:date>2023-06-14T12:43:41Z</dc:date>
    </item>
    <item>
      <title>Re: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669325#M1367</link>
      <description>&lt;P&gt;The memory range from 1FFE_0000 to 1FFF_FFFF is referred as Code TCM and it is only visible in the CM4 memory map, not in the CM7 map. Also in my case, the CMSIS RDDI-DAP driver reports an error when trying to access this memory.&lt;/P&gt;
&lt;P&gt;I'm not an expert for MEM-AP behavior, but this will most likely be caused by an internal bus structure and connection point where the DAP MEM-AP is connected.&lt;/P&gt;
&lt;P&gt;As a workaround, I would recommend to change the linker settings of the CM4 project to use CM4 OCRAM for data (variables) storage.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 12:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669325#M1367</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-06-14T12:51:13Z</dc:date>
    </item>
    <item>
      <title>Re: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669366#M1368</link>
      <description>&lt;P&gt;Thanks Michal for your responses,&lt;BR /&gt;I tried to define a variable in&amp;nbsp;NCACHE_REGION which is in the OCRAM in CM4 core. this variable was incrementing to 1000000 and then set to zero.&lt;BR /&gt;The value in Freemaster was captured as a random number without chaning. it seems changes to variable in CM4 is not reflecting.&lt;BR /&gt;&lt;BR /&gt;I will continue to test more and let you know until we figure that out.&lt;BR /&gt;&lt;BR /&gt;Thanks again for your help.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Jun 2023 13:59:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1669366#M1368</guid>
      <dc:creator>Sam_im</dc:creator>
      <dc:date>2023-06-14T13:59:11Z</dc:date>
    </item>
    <item>
      <title>Re: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1670221#M1369</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;what you describe typically happens when a cache is enabled.&amp;nbsp;The FreeMASTER/JTAG accesses the physical memory storage of the variable which never changes as the variable remains in cache all the time.&lt;/P&gt;
&lt;P&gt;I'd recommend to double check:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;If M4 cache is indeed inhibited in this memory region.&lt;/LI&gt;
&lt;LI&gt;Try to manually flush cache after incrementing the value - just as an experiment&lt;/LI&gt;
&lt;LI&gt;See how CM7 sees the same memory location - this could indicate also how JTAG sees it.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jun 2023 10:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1670221#M1369</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-06-15T10:51:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problem accessing Slave CM4 variables on a multicore master-slave project</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1673663#M1371</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I switched to use only CM7 and pass data between CM7 and CM4. Working with a multicore app is not obviously an option in freemaster.&amp;nbsp;&lt;BR /&gt;Thank you any way MichalH,&lt;/P&gt;</description>
      <pubDate>Wed, 21 Jun 2023 13:04:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Problem-accessing-Slave-CM4-variables-on-a-multicore-master/m-p/1673663#M1371</guid>
      <dc:creator>Sam_im</dc:creator>
      <dc:date>2023-06-21T13:04:15Z</dc:date>
    </item>
  </channel>
</rss>