<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MM9Z1_638 in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/MM9Z1-638/m-p/1664230#M1357</link>
    <description>&lt;LI-SPOILER&gt;Good afternoon. I have an MM9Z1_638 controller which is installed on the board&amp;nbsp;&lt;SPAN&gt;CATL.&amp;nbsp;&lt;/SPAN&gt; &lt;LI-SPOILER&gt;&lt;SPAN&gt;&lt;FONT&gt;Question: Can I connect to this controller without additional cost of money?&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/LI-SPOILER&gt; &lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt; &lt;/LI-SPOILER&gt; &lt;LI-SPOILER&gt;&lt;SPAN&gt;&lt;FONT&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/LI-SPOILER&gt; &lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt; &lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt;</description>
    <pubDate>Tue, 06 Jun 2023 10:08:32 GMT</pubDate>
    <dc:creator>Evgeniyy</dc:creator>
    <dc:date>2023-06-06T10:08:32Z</dc:date>
    <item>
      <title>MM9Z1_638</title>
      <link>https://community.nxp.com/t5/FreeMASTER/MM9Z1-638/m-p/1664230#M1357</link>
      <description>&lt;LI-SPOILER&gt;Good afternoon. I have an MM9Z1_638 controller which is installed on the board&amp;nbsp;&lt;SPAN&gt;CATL.&amp;nbsp;&lt;/SPAN&gt; &lt;LI-SPOILER&gt;&lt;SPAN&gt;&lt;FONT&gt;Question: Can I connect to this controller without additional cost of money?&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/LI-SPOILER&gt; &lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt; &lt;/LI-SPOILER&gt; &lt;LI-SPOILER&gt;&lt;SPAN&gt;&lt;FONT&gt;&amp;nbsp;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/LI-SPOILER&gt; &lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt; &lt;LI-SPOILER&gt;&amp;nbsp;&lt;/LI-SPOILER&gt;</description>
      <pubDate>Tue, 06 Jun 2023 10:08:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/MM9Z1-638/m-p/1664230#M1357</guid>
      <dc:creator>Evgeniyy</dc:creator>
      <dc:date>2023-06-06T10:08:32Z</dc:date>
    </item>
  </channel>
</rss>