<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FreeMASTER USB TAP support for DSC 83xx/E in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-USB-TAP-support-for-DSC-83xx-E/m-p/1626925#M1304</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use FreeMASTER 3.2 for many projects and now I'm going back to work with DSC 56F83xx/E. I have made it through the Classic IDE to Eclipse IDE migration, but finally I'm stucked with the FreeMASTER. In version 2.0, the "Configure" connection settings for JTAG/EOnCE plugin looks different and I'm not able to find out if the FMSTR v3.2 is actually compatible with the USB TAP (in the new-look settings, I cannot see the USB TAP option, just P&amp;amp;E + USB Multilink, which does not work with my USB TAP). The USB TAP itself works fine - I can download the FW and debug.&lt;/P&gt;&lt;P&gt;So my question is: how should I configure the FreeMASTER plugin to work with USB TAP?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
    <pubDate>Mon, 03 Apr 2023 14:23:27 GMT</pubDate>
    <dc:creator>matejpacha_Ineltech</dc:creator>
    <dc:date>2023-04-03T14:23:27Z</dc:date>
    <item>
      <title>FreeMASTER USB TAP support for DSC 83xx/E</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-USB-TAP-support-for-DSC-83xx-E/m-p/1626925#M1304</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use FreeMASTER 3.2 for many projects and now I'm going back to work with DSC 56F83xx/E. I have made it through the Classic IDE to Eclipse IDE migration, but finally I'm stucked with the FreeMASTER. In version 2.0, the "Configure" connection settings for JTAG/EOnCE plugin looks different and I'm not able to find out if the FMSTR v3.2 is actually compatible with the USB TAP (in the new-look settings, I cannot see the USB TAP option, just P&amp;amp;E + USB Multilink, which does not work with my USB TAP). The USB TAP itself works fine - I can download the FW and debug.&lt;/P&gt;&lt;P&gt;So my question is: how should I configure the FreeMASTER plugin to work with USB TAP?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Matej&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 14:23:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-USB-TAP-support-for-DSC-83xx-E/m-p/1626925#M1304</guid>
      <dc:creator>matejpacha_Ineltech</dc:creator>
      <dc:date>2023-04-03T14:23:27Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER USB TAP support for DSC 83xx/E</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-USB-TAP-support-for-DSC-83xx-E/m-p/1629073#M1308</link>
      <description>&lt;P&gt;Ahoj Mateji,&lt;/P&gt;
&lt;P&gt;the USB TAP for DSCs is no not supported by FreeMASTER 3.x versions. I do recommend to use P&amp;amp;E Multilink Universal configured for the DSC JTAG access. This one is tested with the FreeMASTER JTAG/EOnCE plug-in.&lt;/P&gt;
&lt;P&gt;I also recommend to use the latest freemaster driver code released recently for the MC56F83000-EVK at the&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/en/select" target="_self"&gt;MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;site.&lt;/P&gt;
&lt;P&gt;Actually adding a support for USBTAP device back to FreeMASTER 3.2 is on our to do list, but it is not for next few months.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Apr 2023 11:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-USB-TAP-support-for-DSC-83xx-E/m-p/1629073#M1308</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2023-04-06T11:41:12Z</dc:date>
    </item>
    <item>
      <title>Re: FreeMASTER USB TAP support for DSC 83xx/E</title>
      <link>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-USB-TAP-support-for-DSC-83xx-E/m-p/1629180#M1310</link>
      <description>Ahoj Michale,&lt;BR /&gt;good to know. Right now I have switched to FreeMASTER over CAN with no major issues. For the future it would be great to have the USB TAP support back in FMSTR.&lt;BR /&gt;&lt;BR /&gt;Actually, we have to use the old QucikStart-based codes just to avoid another round of development from scratch. There are still some challenges, but in general it seems we can live with the CW 11.&lt;BR /&gt;&lt;BR /&gt;Měj se!</description>
      <pubDate>Thu, 06 Apr 2023 14:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/FreeMASTER-USB-TAP-support-for-DSC-83xx-E/m-p/1629180#M1310</guid>
      <dc:creator>matejpacha_Ineltech</dc:creator>
      <dc:date>2023-04-06T14:06:10Z</dc:date>
    </item>
  </channel>
</rss>