<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTER中的主题 Re: Issue with Array Viewer</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1521710#M1163</link>
    <description>&lt;P&gt;Dear Luca,&lt;/P&gt;
&lt;P&gt;yes the issue is now fixed and will be part of the November release. If you are willing to test the patch, please reach out to me directly at &lt;A href="mailto:michal.hanak@nxp.com" target="_blank"&gt;michal.hanak@nxp.com&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
    <pubDate>Wed, 14 Sep 2022 06:26:05 GMT</pubDate>
    <dc:creator>MichalH</dc:creator>
    <dc:date>2022-09-14T06:26:05Z</dc:date>
    <item>
      <title>Issue with Array Viewer</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1510900#M1139</link>
      <description>&lt;P&gt;Hi, I am trying to use the Array Viewer feature, to read a 2MB of external RAM interpreted as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;__attribute__ ((section (".ram_ext"))) FMSTR_U8 fmstrapp_arrayview_buffer[2000000];&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So I created an Array Viewer with &lt;STRONG&gt;fmstrapp_arrayview_buffer[0]&lt;/STRONG&gt; as a variable, and then I set the length of the array to 2000000.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But something is going wrong. In the code I set all array elements to 255 (and I can confirm they are set from the debugger, as well as from the freemaster watch window). But the Array Viewer will only catch the first 2% of the values. The rest is just zeros:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lucabarbiero_0-1661341578274.png" style="width: 736px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/191134i9169EFDF94F6B793/image-dimensions/736x275?v=v2" width="736" height="275" role="button" title="lucabarbiero_0-1661341578274.png" alt="lucabarbiero_0-1661341578274.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Same issue if I try with a 200 KB array in internal RAM, and regardless of the communication channel (tested with TCP and PDBDM)&lt;/P&gt;&lt;P&gt;Any idea?&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Aug 2022 11:54:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1510900#M1139</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2022-08-24T11:54:16Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with Array Viewer</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1511015#M1143</link>
      <description>&lt;P&gt;Hello Luca,&lt;/P&gt;
&lt;P&gt;issue confirmed. The ArrayViewer will only read up to 64kB. Larger sizes will cause premature stop and zero-fill of the rest of the buffer.&lt;/P&gt;
&lt;P&gt;We will focus to get it fixed asap.&lt;/P&gt;
&lt;P&gt;Thanks for a good catch (as usual),&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Aug 2022 14:43:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1511015#M1143</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-08-24T14:43:56Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with Array Viewer</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1521319#M1162</link>
      <description>&lt;P&gt;Hi Michal, were you able to fix this, and do you know when you will release the next freemaster version?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Luca&lt;/P&gt;</description>
      <pubDate>Tue, 13 Sep 2022 14:25:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1521319#M1162</guid>
      <dc:creator>lucabarbiero</dc:creator>
      <dc:date>2022-09-13T14:25:26Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with Array Viewer</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1521710#M1163</link>
      <description>&lt;P&gt;Dear Luca,&lt;/P&gt;
&lt;P&gt;yes the issue is now fixed and will be part of the November release. If you are willing to test the patch, please reach out to me directly at &lt;A href="mailto:michal.hanak@nxp.com" target="_blank"&gt;michal.hanak@nxp.com&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 06:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1521710#M1163</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-09-14T06:26:05Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with Array Viewer</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1566653#M1217</link>
      <description>&lt;P&gt;Hello Luca,&lt;/P&gt;
&lt;P&gt;this issue is now fixed in version 3.2.1.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Thu, 08 Dec 2022 07:45:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Issue-with-Array-Viewer/m-p/1566653#M1217</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-12-08T07:45:00Z</dc:date>
    </item>
  </channel>
</rss>