<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックFreemaster 3.2 - Chromium Embedded Framework uses CORS after update</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Chromium-Embedded-Framework-uses-CORS-after/m-p/1499346#M1086</link>
    <description>&lt;P&gt;We are using Freemaster to access data on our sharepoint and SQL database.&lt;BR /&gt;After the update to from version 3.1 to version 3.2 this is no longer possible.&lt;BR /&gt;After several tests I am pretty sure that it has to do with CORS.&lt;BR /&gt;Are there any information if and why it was enabled for the Freemaster version 3.2 or is this just a bug?&lt;BR /&gt;Is there a way to disable CORS?&lt;/P&gt;</description>
    <pubDate>Tue, 02 Aug 2022 07:51:47 GMT</pubDate>
    <dc:creator>M4k5</dc:creator>
    <dc:date>2022-08-02T07:51:47Z</dc:date>
    <item>
      <title>Freemaster 3.2 - Chromium Embedded Framework uses CORS after update</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Chromium-Embedded-Framework-uses-CORS-after/m-p/1499346#M1086</link>
      <description>&lt;P&gt;We are using Freemaster to access data on our sharepoint and SQL database.&lt;BR /&gt;After the update to from version 3.1 to version 3.2 this is no longer possible.&lt;BR /&gt;After several tests I am pretty sure that it has to do with CORS.&lt;BR /&gt;Are there any information if and why it was enabled for the Freemaster version 3.2 or is this just a bug?&lt;BR /&gt;Is there a way to disable CORS?&lt;/P&gt;</description>
      <pubDate>Tue, 02 Aug 2022 07:51:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Chromium-Embedded-Framework-uses-CORS-after/m-p/1499346#M1086</guid>
      <dc:creator>M4k5</dc:creator>
      <dc:date>2022-08-02T07:51:47Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster 3.2 - Chromium Embedded Framework uses CORS after update</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Chromium-Embedded-Framework-uses-CORS-after/m-p/1500024#M1088</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I suppose you were using the CEF (Chromium) to render your pages in FreeMASTER. The version 3.2 brings the new version of CEF (99.2.10+gfecf7ca+chromium-99.0.4844.51) - so I suspect the change in CORS handling might be related to this update. FreeMASTER itself does not do anything special about page sources, origins and redirects. (Well, it &lt;EM&gt;does&lt;/EM&gt;, but only a minimum needed to handle a special fmstr:// protocol which fetches files from the target board).&lt;/P&gt;
&lt;P&gt;The FreeMASTER version 3.2 also brings the Microsoft Edge WebView2 component which is also chromium based. Can you try the behavior in this browser?&lt;/P&gt;
&lt;P&gt;If this does not work, please describe your problem case in more details, so we could repeat the issue locally.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;BR /&gt;Michal&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 06:49:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-3-2-Chromium-Embedded-Framework-uses-CORS-after/m-p/1500024#M1088</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-08-03T06:49:32Z</dc:date>
    </item>
  </channel>
</rss>