<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックFreemaster Board not detected error</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Board-not-detected-error/m-p/1494314#M1071</link>
    <description>&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I am running a modified model of pmsm closed loop control . the model was running fine in freemaster till yesterday but now the connection is getting disconnected frequently and when i try to connect it again it shows no board detected error.&lt;/P&gt;&lt;P&gt;I have attached the slx file of the model&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 23 Jul 2022 10:41:27 GMT</pubDate>
    <dc:creator>Sriram</dc:creator>
    <dc:date>2022-07-23T10:41:27Z</dc:date>
    <item>
      <title>Freemaster Board not detected error</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Board-not-detected-error/m-p/1494314#M1071</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;I am running a modified model of pmsm closed loop control . the model was running fine in freemaster till yesterday but now the connection is getting disconnected frequently and when i try to connect it again it shows no board detected error.&lt;/P&gt;&lt;P&gt;I have attached the slx file of the model&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 23 Jul 2022 10:41:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Board-not-detected-error/m-p/1494314#M1071</guid>
      <dc:creator>Sriram</dc:creator>
      <dc:date>2022-07-23T10:41:27Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster Board not detected error</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Board-not-detected-error/m-p/1494677#M1072</link>
      <description>&lt;P&gt;Dear &lt;SPAN&gt;Sriram&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;if FreeMASTER was working earlier, you need to focus at the changes you made in the application code. It is out of scope of this forum to analyze your code, I can only give you some general comments.&amp;nbsp; You can also send more information about your customization of the motor control application to the &lt;A href="https://community.nxp.com/t5/Motor-Control-and-Smart-Energy/bd-p/motor-control-and-smart-energy" target="_self"&gt;dedicated motor-control community&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;General reasons why FreeMASTER can become un-responsive when using a serial line:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Application main-loop gets too busy and FreeMASTER operates in a polled mode (FMSTR_POLL_DRIVEN). A solution may be to use interrupt-driven communication or to lower the communication baudrate.&lt;/LI&gt;
&lt;LI&gt;System overload - if application is spending too much time in interrupts, not leaving enough of run time to communication processing.&lt;/LI&gt;
&lt;LI&gt;FreeMASTER reads a different ELF file than actually running in the MCU. This would cause the variables to be read from different addresses. A solution would be to reload proper ELF file or use the TSA runtime symbolic tables.&lt;/LI&gt;
&lt;LI&gt;System clock, pins or other configuration changes, resulting in UART becomes misconfigured.&lt;/LI&gt;
&lt;LI&gt;Physical damage of the chip (?) Does the FreeMASTER work better if you try your "yesterday's" version? If not, then a physical damage could be relevant.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Michal&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 09:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Board-not-detected-error/m-p/1494677#M1072</guid>
      <dc:creator>MichalH</dc:creator>
      <dc:date>2022-07-25T09:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster Board not detected error</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-Board-not-detected-error/m-p/1494695#M1073</link>
      <description>&lt;P&gt;freemaster runs fine on previous versions of my model so i think the hardware is fine&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 09:22:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-Board-not-detected-error/m-p/1494695#M1073</guid>
      <dc:creator>Sriram</dc:creator>
      <dc:date>2022-07-25T09:22:46Z</dc:date>
    </item>
  </channel>
</rss>