<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using communication plugins with mcbcom in FreeMASTER</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Using-communication-plugins-with-mcbcom/m-p/1491799#M1063</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203832"&gt;@Haitham_Ismail&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you using the mcbcom.dll from FreeMASTER or FreeMASTER Lite folder. There is slight difference in the way each library handles the plugins.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The one located in FreeMASTER uses uses plugin CLSID register in Windows system. You need to use&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;&lt;SPAN class=""&gt;6D13CD9D-9F2D-4066-B655-45B54CA7494B &lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/EM&gt;&lt;SPAN class=""&gt;i&lt;/SPAN&gt;nstead of &lt;EM&gt;&lt;STRONG&gt;NET&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt;key in the connection string&lt;/LI&gt;
&lt;LI&gt;The one located in FreeMASTER Lite folder uses a relative path and a friendly name. Your connection string should work with Fmstr Lite dll, but you need to include &lt;EM&gt;&lt;STRONG&gt;plugins&lt;/STRONG&gt; &lt;/EM&gt;folder next to the dll because of the relative path discovery.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Kind regards,&lt;BR /&gt;Iulian&lt;/P&gt;</description>
    <pubDate>Tue, 19 Jul 2022 12:47:59 GMT</pubDate>
    <dc:creator>iulian_stan</dc:creator>
    <dc:date>2022-07-19T12:47:59Z</dc:date>
    <item>
      <title>Using communication plugins with mcbcom</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Using-communication-plugins-with-mcbcom/m-p/1491126#M1062</link>
      <description>&lt;P&gt;I am trying to develop a 3rd party application that uses the mcbcom library. I am using the TCP plugin for the project. I already tested the setup with TCP plugin using FreeMASTER desktop and FreeMaster lite and it works as intended. However, when I use the mcbcom library in the application I get an "Error occurred" (code 0x80000000). I am using imxrt 1050 board and here is the connection string&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;"NET;169.254.120.174;type=TCP;port=3344;timeout=500"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;So I was wondering what are the implementations of the communication plugins in the mcbcom library.&lt;BR /&gt;&lt;BR /&gt;Thanks in advance&lt;BR /&gt;&lt;BR /&gt;PS: I know that it is not from the rest of the code since I tested it on USB CDC &amp;amp; LPUART connections first&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 18 Jul 2022 15:20:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Using-communication-plugins-with-mcbcom/m-p/1491126#M1062</guid>
      <dc:creator>Haitham_Ismail</dc:creator>
      <dc:date>2022-07-18T15:20:27Z</dc:date>
    </item>
    <item>
      <title>Re: Using communication plugins with mcbcom</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Using-communication-plugins-with-mcbcom/m-p/1491799#M1063</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203832"&gt;@Haitham_Ismail&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Are you using the mcbcom.dll from FreeMASTER or FreeMASTER Lite folder. There is slight difference in the way each library handles the plugins.&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The one located in FreeMASTER uses uses plugin CLSID register in Windows system. You need to use&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;&lt;SPAN class=""&gt;6D13CD9D-9F2D-4066-B655-45B54CA7494B &lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/EM&gt;&lt;SPAN class=""&gt;i&lt;/SPAN&gt;nstead of &lt;EM&gt;&lt;STRONG&gt;NET&amp;nbsp;&lt;/STRONG&gt;&lt;/EM&gt;key in the connection string&lt;/LI&gt;
&lt;LI&gt;The one located in FreeMASTER Lite folder uses a relative path and a friendly name. Your connection string should work with Fmstr Lite dll, but you need to include &lt;EM&gt;&lt;STRONG&gt;plugins&lt;/STRONG&gt; &lt;/EM&gt;folder next to the dll because of the relative path discovery.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Kind regards,&lt;BR /&gt;Iulian&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jul 2022 12:47:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Using-communication-plugins-with-mcbcom/m-p/1491799#M1063</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2022-07-19T12:47:59Z</dc:date>
    </item>
  </channel>
</rss>