<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>FreeMASTERのトピックRe: Freemaster lite &amp;quot;GetRecorderStatus&amp;quot; can return value 0x05 ?</title>
    <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-lite-quot-GetRecorderStatus-quot-can-return-value/m-p/1471360#M1036</link>
    <description>&lt;P&gt;Hi Iulian,&lt;/P&gt;&lt;P&gt;Yes, I am getting response '&lt;STRONG&gt;4&lt;/STRONG&gt;' for only samples less than or equal to '100' (When set in recorder config under '&lt;STRONG&gt;pointsTotal&lt;/STRONG&gt;') and it was &lt;STRONG&gt;not stable&lt;/STRONG&gt; ( sometimes getting '2' even).&lt;/P&gt;&lt;P&gt;---But after increasing samples more than '100', the response code is always '4'.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gohith&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 09 Jun 2022 09:29:11 GMT</pubDate>
    <dc:creator>UserTetraWise</dc:creator>
    <dc:date>2022-06-09T09:29:11Z</dc:date>
    <item>
      <title>Freemaster lite "GetRecorderStatus" can return value 0x05 ?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-lite-quot-GetRecorderStatus-quot-can-return-value/m-p/1470555#M1031</link>
      <description>&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;On performing Freemaster Lite and using method&amp;nbsp; &lt;STRONG&gt;GetRecorderStatus, &lt;/STRONG&gt;I tested for multiple scenarios and got the values 0, 2, and 4 back as expected but not 5 even the data is ready (I assumed because of checking the samples after download)&lt;/P&gt;&lt;P&gt;later using &lt;STRONG&gt;GetRecorderData&amp;nbsp;&lt;/STRONG&gt;to download. Am I missing something here ?&lt;/P&gt;&lt;P&gt;(Using Python Script)&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Gohith Kanchinatham&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 09:37:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-lite-quot-GetRecorderStatus-quot-can-return-value/m-p/1470555#M1031</guid>
      <dc:creator>UserTetraWise</dc:creator>
      <dc:date>2022-06-08T09:37:39Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster lite "GetRecorderStatus" can return value 0x05 ?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-lite-quot-GetRecorderStatus-quot-can-return-value/m-p/1470817#M1034</link>
      <description>&lt;P&gt;Hi Gohith,&lt;/P&gt;&lt;P&gt;I went though FreeMASTER library and noticed that the status codes were updated, but this was not reflected in the documentation. Correct status codes are as follows:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;0 - not configured
1 - configured, stopped, no-data
2 - running
3 - stopped, not enough data sampled (previously was 4)
4 - stopped, data ready (previously was 5)&lt;/LI-CODE&gt;&lt;P&gt;You are getting correct status codes but their meaning is mismatched. We will update the documentation accordingly.&lt;/P&gt;&lt;P&gt;Apologies for the&amp;nbsp;inconvenience,&lt;BR /&gt;Iulian&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 08 Jun 2022 16:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-lite-quot-GetRecorderStatus-quot-can-return-value/m-p/1470817#M1034</guid>
      <dc:creator>iulian_stan</dc:creator>
      <dc:date>2022-06-08T16:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: Freemaster lite "GetRecorderStatus" can return value 0x05 ?</title>
      <link>https://community.nxp.com/t5/FreeMASTER/Freemaster-lite-quot-GetRecorderStatus-quot-can-return-value/m-p/1471360#M1036</link>
      <description>&lt;P&gt;Hi Iulian,&lt;/P&gt;&lt;P&gt;Yes, I am getting response '&lt;STRONG&gt;4&lt;/STRONG&gt;' for only samples less than or equal to '100' (When set in recorder config under '&lt;STRONG&gt;pointsTotal&lt;/STRONG&gt;') and it was &lt;STRONG&gt;not stable&lt;/STRONG&gt; ( sometimes getting '2' even).&lt;/P&gt;&lt;P&gt;---But after increasing samples more than '100', the response code is always '4'.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gohith&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jun 2022 09:29:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/FreeMASTER/Freemaster-lite-quot-GetRecorderStatus-quot-can-return-value/m-p/1471360#M1036</guid>
      <dc:creator>UserTetraWise</dc:creator>
      <dc:date>2022-06-09T09:29:11Z</dc:date>
    </item>
  </channel>
</rss>