<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>eIQ Machine Learning SoftwareのトピックRe: Deepview RT. Comminucating with target MIMXRT1170 EVB</title>
    <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Deepview-RT-Comminucating-with-target-MIMXRT1170-EVB/m-p/1554923#M634</link>
    <description>&lt;P&gt;Hello marc, to load a model, you need to use the ModelClient API, as described in the DeepViewRT documentation. The application doesn't support a simple curl call to upload a new model.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
    <pubDate>Wed, 16 Nov 2022 12:52:30 GMT</pubDate>
    <dc:creator>david_piskula</dc:creator>
    <dc:date>2022-11-16T12:52:30Z</dc:date>
    <item>
      <title>Deepview RT. Comminucating with target MIMXRT1170 EVB</title>
      <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Deepview-RT-Comminucating-with-target-MIMXRT1170-EVB/m-p/1540596#M631</link>
      <description>&lt;P&gt;This is for mcuxpresso project application evkmimxrt1170_deepviewrt_modelrunner_cm7 loaded on the target.&lt;BR /&gt;Is there a curl command to download a model_file.rtm to the target?&lt;BR /&gt;Similar to the curl command used to download an image.jpg and run infer.&lt;BR /&gt;curl -D - -XPOST -H 'Accept: text/plain' -H 'Content-Type: image/*' --data-binary '@shark.jpg' '&lt;A href="http://192.168.1.51:10818/v1?run=1" target="_blank"&gt;http://192.168.1.51:10818/v1?run=1&lt;/A&gt;'&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 00:37:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Deepview-RT-Comminucating-with-target-MIMXRT1170-EVB/m-p/1540596#M631</guid>
      <dc:creator>marc_nxp_community</dc:creator>
      <dc:date>2022-10-20T00:37:11Z</dc:date>
    </item>
    <item>
      <title>Re: Deepview RT. Comminucating with target MIMXRT1170 EVB</title>
      <link>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Deepview-RT-Comminucating-with-target-MIMXRT1170-EVB/m-p/1554923#M634</link>
      <description>&lt;P&gt;Hello marc, to load a model, you need to use the ModelClient API, as described in the DeepViewRT documentation. The application doesn't support a simple curl call to upload a new model.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Wed, 16 Nov 2022 12:52:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/eIQ-Machine-Learning-Software/Deepview-RT-Comminucating-with-target-MIMXRT1170-EVB/m-p/1554923#M634</guid>
      <dc:creator>david_piskula</dc:creator>
      <dc:date>2022-11-16T12:52:30Z</dc:date>
    </item>
  </channel>
</rss>